×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 22344041, Entry date: 01/05/2006
(0)
Rate

CP 343-1 Firmware Update V2.1 (6GK7343-1GX11-0XE0)

  • Entry
  • Associated product(s)

The module with order no. 6GK7343-1GX11-0XE0 is now being shipped with new firmware version V2.1. The firmware can be downloaded free of charge.
 

The module with order no. 6GK7343-1GX11-0XE0 is now being shipped with new firmware version V2.1 (succeeds V2.0). Existing CP 343-1IT modules (6GK7343-1GX11-0XE0) with earlier firmware versions can be upgraded by means of a free firmware update (download ID: !22342617!). 
In STEP7 the module can still be configured as firmware version 2.0.

The following product improvements were introduced: 

  - Fetch & Write connections are now re-established in spite of protocol violations.
  - Write command with data length=0 are rejected with error code (error code=6).
  - Problems with BSEND, BRECV, PUT, GET, USEND & URECV have been corrected: High stability in the case of CP STOP/RUN transitions, endlessly executed commands, no loss of performance when the connection is cut by an OPC Server. 
  - Stable against broadcast storms. All connections are re-established afterwards.
  - CP Startup problem corrected.
  - Counters for broadcast and multicast packages now work correctly.
  - MAC and IP addresses are conserved after an overall reset.
  - NTP Client will now also accept servers with versions lower than 4.
  - An incorrect DNS frame will now be handled correctly and no longer lead to to consequential errors.
  - FTP Client: Access to a server file DB in the CP will now work with the full path specification. Example: STOR /cpu1/cpu1db20
  - FTP Server: Connection establishement to the FTP server in "Passive mode" will now also work when operated with the default MAC address.
  - Improvement of the file system with respect to uniform wear of the flash sectors in the case of write events.
 

  Added functions:
  - Display of the variables on a PG now also possible in the CP mode "STOP"

  - The FTP command "DIR File name" is now available. (up to now only "DIR" and "DIR Path")

 

We advise you to upgrade your CP 343-1IT (6GK7343-1GX11-0XE0) with this new firmware.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.