×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22405932, Entry date: 04/19/2006
(0)
Rate

How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?

  • Entry
  • Associated product(s)

Instructions:
You are using the Bürkert pneumatic modules described at the link
http://us.burkert.com
and would like to operate these after an ET 200S IM 151. There are various configuration methods for this depending on the header module.

IM 151-1
For configuring the IM 151-1 as DP slave you use the GSD file that you can download in Entry ID 652154. This contains the Bürkert pneumatic modules that can be operated in the ET 200S.
In STEP 7 you configure the ET 200S from the hardware catalog folder PROFIBUS DP > Other Field Devices > I/O > ET 200S > ET 200S (IM 151) as in Fig. 1:


Fig. 01
 
 

IM 151-3 PN
You can configure the Bürkert pneumatic modules in the IM 151-3 PN using the PROFINET GSD file.
In STEP 7 HW Config take the ET 200S from the hardware catalog folder PROFINET IO > I/O > ET 200S > IM 151-3 PN
and configure the Bürkert modules from the Pneumatic folder as in Fig. 2:


Fig. 02
 
 

Note
At the moment the Bürkert pneumatic modules can only be used in the interface modules (IM 151) of the ET 200S distributed I/O system mentioned above.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.