×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 22445076, Entry date: 04/27/2006
(1)
Rate

STEP 7 V5.4 Released for Delivery

  • Entry
  • Associated product(s)


STEP 7 V5.4
has been released for immediate delivery. An upgrade is available at a charge. Users with a valid Software Update Service agreement for STEP 7 will receive the upgrade for STEP 7 V5.4 automatically. STEP 7 V5.4 will also be included in the new STEP 7 Professional Edition 2006, with start of delivery planned for end of April 2006. We will inform you accordingly.


Contents:

  1. Ordering data for STEP 7 V5.4
  2. System prerequisites
  3. Overhead slides "STEP 7 V5.4 - Highlights of the new STEP 7 version"
  4. Compatibility
  5. STEP 7 V5.3 – Product phaseout
  6. STEP 7 V5.2 – Product discontinuation

1. Ordering data for STEP 7 V5.4

Order No.

Designation

6ES7810-4CC08-0YA5

SIMATIC S7, STEP7 V5.4
FLOATING LICENSE FOR 1 USER

6ES7810-4CC08-0YE5

SIMATIC S7, STEP7 V5.4 UPGRADE (V3.X - V5.3 to V5.4)
FLOATING LICENSE FOR 1 USER

6ES7810-4CC08-0YA6

SIMATIC S7, STEP7 V5.4
RENTAL LICENSE FOR 50 HOURS

6ES7810-4CC08-0YA7

SIMATIC S7, STEP7 V5.4,
DATA CARRIER INC.TRIAL LICENSE,

6ES7810-4BC01-0YX2

SIMATIC S7, STEP7 SOFTWARE UPDATE SERVICE FOR 1 YEAR WITH AUTOM. EXTENSION, LATEST SOFTWARE VERSION IS A PRECONDITION


STEP 7 V5.4 Upgrade:

Clients who use STEP 7 V3.x, V4.x, V5.0, V5.1, V5.2 or V5.3 already, can buy the upgrade at a charge. The precondition for the installation of the upgrade package is a valid license for STEP 7 V3.x, V4.x, V5.0, V5.1, V5.2 or V5.3.
 

STEP 7 V5.4 Rental License:

Clients who only use STEP 7 only occasionally can make use of this license form with an operating time of 50 hrs. The time starts running when STEP 7 is started up, and counting stops when STEP 7 is stopped.
A transition to standby mode with STEP 7 started is not counted as termination of STEP 7.

STEP 7 V5.4 Trial License:

For clients who wish to learn more about STEP 7. The Trial License will run for 14 days, beginning from the first start of STEP 7. During this time the software has its full functionality.

General:

STEP 7 V5.4 is supplied on CD ROM; The license is supplied on FD.
STEP 7 is multilingual (G, E, F, I, Sp).

Documentation:

The documentation for STEP 7 (Basic Information and Reference Manuals) is supplied in the form of a PDF file on the product CD ROM. It is also available in printed form.

The printed version of the Basic Information (includes: Getting Started, User manuals for HW Configuration, programming and changeover from S5):  

Order No.

Designation

6ES7810-4CA08-8AW0

BASIC INFORMATION for V5.4, German

6ES7810-4CA08-8BW0

BASIC INFORMATION for V5.4, English

6ES7810-4CA08-8CW0

BASIC INFORMATION for V5.4, French

6ES7810-4CA08-8DW0

BASIC INFORMATION for V5.4, Spanish

6ES7810-4CA08-8EW0

BASIC INFORMATION for V5.4, Italian

The printed version of the Reference Manual (includes: User manual for STL/LAD/FBD and Reference Manual for S7-300/400):

Order No.

Designation

6ES7810-4CA08-8AW1

REFERENCE MANUAL for V5.4, GERMAN

6ES7810-4CA08-8BW1

REFERENCE MANUAL for V5.4, ENGLISH

6ES7810-4CA08-8CW1

REFERENCE MANUAL for V5.4, FRENCH

6ES7810-4CA08-8DW1

REFERENCE MANUAL for V5.4, SPANISH

6ES7810-4CA08-8EW1

REFERENCE MANUAL for V5.4, ITALIAN

 

2. System prerequisites

Supported operating systems:

  • MS Windows 2000 Professional (SP4)
  • MS Windows XP Professional  (SP1, SP1a or SP2)
  • MS Windows Server 2003 with or without SP1, as workstation computer
    (not released for SIMATIC M7)

Note:
The precondition for all operating systems is the Microsoft Internet Explorer 6.0 (or higher).
Windows 95 / 98 / Me and NT are no longer supported.

3. Set of overhead slides "STEP 7 V5.4 - Highlights of the new STEP 7 version"

We have summarized the information on STEP 7 V5.4 in a set of overhead slides

STEP 7 V5.4 - Highlights of the new version

For ordering data on SIMATIC Logon please see entry ID: 22560024

4. Compatibility

General:

  • STEP 7 V5.4 is fully upwardly compatible with STEP 7 V5.3, V5.2, V5.1, V5.0, V4.x and V3.x, i.e. Programs and projects created with these versions can be further processed with STEP 7 V5.4 without any changes.
  • STEP 7 V5.3 is also reverse compatible with these versions under the condition that a V5.4 project does not contain any components and functions that are not supported by STEP 7 V5.3, V5.2, V5.1, V5.0, V4.x or V3.x, e.g. the new CPUs or new functions.
    • If a project created with STEP 7 V5.4 is to be further processed with STEP 7 V5.0, for example, the V5.4 project may only contain module order no.’s known to STEP 7 V5.0. Where necessary, new modules should be configured with the "predecessor order no.".
    • This is not applicable down to STEP 7 V5.1 incl. SP3, because here new and unknown modules can also be depicted.
  • As from STEP 7 V5.2 onwards, many new modules can be "post loaded".

5. STEP 7 V5.3 - Product phaseout

With the release of STEP 7 V5.4, STEP 7 V5.3 has been declared a mature product. This means that the relevant items will be deleted from the catalog, but will nevertheless remain available for normal ordering for aprrox. one more year:

Order No.

Designation

6ES7810-4CC07-0YA5

SIMATIC S7, STEP7 V5.3
FLOATING LICENSE FOR 1 USER

6ES7810-4CC07-0YE5

SIMATIC S7, STEP7 V5.3
UPGRADE (V3.X - V5.2 to V5.3)
FLOATING LICENSE FOR 1 USER

6ES7810-4CC07-0YC5

SIMATIC S7, STEP7 V5.3 POWERPACK
(STEP 7 LITE V2.0 to STEP 7 V5.3)
FLOATING LICENSE FOR 1 USER

6ES7810-4CC07-0YA6

SIMATIC S7, STEP7 V5.3
RENTAL LICENSE FOR 50 HOURS

6ES7810-4CC07-0YA7

SIMATIC S7, STEP7 V5.3,
DATA CARRIER INC.TRIAL LICENSE,

6ES7810-4CA07-8AW0

BASIC INFORMATION for V5.3, German

6ES7810-4CA07-8BW0

BASIC INFORMATION for V5.3, English

6ES7810-4CA07-8CW0

BASIC INFORMATION for V5.3, French

6ES7810-4CA07-8DW0

BASIC INFORMATION for V5.3, Spanish

6ES7810-4CA07-8EW0

BASIC INFORMATION for V5.3, Italian

6ES7810-4CA07-8AW1

REFERENCE MANUAL for V5.3, GERMAN

6ES7810-4CA07-8BW1

REFERENCE MANUAL for V5.3, ENGLISH

6ES7810-4CA07-8CW1

REFERENCE MANUAL for V5.3, FRENCH

6ES7810-4CA07-8DW1

REFERENCE MANUAL for V5.3, SPANISH

6ES7810-4CA07-8EW1

REFERENCE MANUAL for V5.3, ITALIAN

 

The coloured order numbers were updated at December 11-2006

 

6. STEP 7 V5.2 - Product discontinuation

The supply of STEP 7 V5.2 has been discontinued with immediate effect. This means that STEP 7 V5.2 and the associated manuals are no longer available. The following products are affected by this measure:

Order No.

Designation

6ES7810-4CC06-0YX0

SIMATIC S7, STEP7 V5.2
SINGLE LICENSE FOR 1 INSTALLATION

6ES7810-4CC06-0YX4

SIMATIC S7, STEP7 V5.2
UPGRADE (V3.X - V5.1 to V5.2)
SINGLE LICENSE FOR 1 INSTALLATION

6ES7810-4CC06-0YX5

SIMATIC S7, STEP7 V5.2 POWERPACK
(STEP 7 LITE V2.0 to STEP 7 V5.2)
SINGLE LICENSE FOR 1 INSTALLATION

6ES7810-4CA06-8AA0

BASIC INFORMATION for V5.2, German

6ES7810-4CA06-8BA0

BASIC INFORMATION for V5.2, English

6ES7810-4CA06-8CA0

BASIC INFORMATION for V5.2, French

6ES7810-4CA06-8DA0

BASIC INFORMATION for V5.2, Spanish

6ES7810-4CA06-8EA0

BASIC INFORMATION for V5.2, Italian

6ES7810-4CA06-8AR0

REFERENCE MANUAL for V5.2, GERMAN

6ES7810-4CA06-8BR0

REFERENCE MANUAL for V5.2, ENGLISH

6ES7810-4CA06-8CR0

REFERENCE MANUAL for V5.2, FRENCH

6ES7810-4CA06-8DR0

REFERENCE MANUAL for V5.2, SPANISH

6ES7810-4CA06-8ER0

REFERENCE MANUAL for V5.2, ITALIAN



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.