×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 22497240, Entry date: 01/03/2006
(0)
Rate

MCIS, DCOM settings with ADDM Agent V1 installation.

  • Entry
  • Associated product(s)

QUESTION:
When installing ADDM Agent V1, the installation stops at 87% and setup cannot be terminated.

ANSWER:
The Microsoft Installer is used for the ADDM installation setup. MS Installer requires certain DCOM settings.

The DCOM settings are reached as follows:
Start -> Run : dcomcnfg

The following settings under Default Properties are required:
- Enable Distributed COM on this Computer - activated (check mark is set)
- Default Authentication Level: Connect
- Default Impersonation Level: Identify

Terminate the setup via the Task Manager, make the DCOM settings as described above, reboot the system and then restart the setup.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.