×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22548889, Entry date: 01/22/2008
(0)
Rate

Which cable can you use for data transfer between a Micro Panel and a configuration PC?

  • Entry
  • Associated product(s)

Configuration Notes:
Data transfer (Image Update, Project Download and Backup/Restore) between a configuration PC and a Micro Panel is only possible via a PC/PPI cable.

The following PC/PPI cables are available:

  • USB/PPI multimaster cable
  • RS232/PPI multimaster cable

USB/PPI multimaster cable
The USB/PPI multimaster cable is released as from "E-Stand" 05 and WinCC flexible 2005 SP1. Please note that not all Micro Panels support data transfer via the USB/PPI multimaster cable. Information on cables that can be used with each of the panels is available in the relevant manual or in Entry ID 19109408.

RS232/PPI multimaster cable
You can use all RS232/PPI multimaster cables (the old ones too) which support a conversion from RS232 to RS485.

The figure shows the connection from the operator panel to the configuration computer.


Fig. 01

 

When using the RS232/PPI multimaster cable (order number: 6ES7901-3CB30-0XA0), you must make sure that DIP switch 5 is set to 0. All other DIP switches are not relevant for transferring projects to a panel.

The figure shows the DIP switches of the RS232/PPI multimaster cable.


Fig. 02

Note:
The RS232/PPI multimaster cable with order numbers 6ES7901-3BF21-0XA0 and 6ES7901-3BF20-0XA0 can still be used.

Links to other topics
More information on this topic is available in the Entry IDs given below:
 

No. Topic Entry ID
1. Manual (OP73micro & TP177micro)
Chapter - Updating the operating system
Entry ID: 21086325
2. Settings on the PC/PPI cables Entry ID: 16810372
Entry ID: 16532946
3. Operating system update in ProTool, ProTool/Pro and WinCC flexible Entry ID: 19701610
4. What transfer options are available in the various operator panels? Entry ID: 19109408

Keywords:
Project transfer, Transfer, Project download

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.