×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 22564754, Entry date: 01/22/2013
(1)
Rate

Which ET 200S modules support the option handling function?

  • Entry
  • Associated product(s)

Description
A distinction is made between the function Option handling with reserve module and Option handling without reserve module. In the following table, there is information on which interface modules support option handling with or without reserve modules.
 

Interface modules Option handling with reserve module Option handling without reserve module
IM151-1 STANDARD
6ES7151-1AA03-0AB0
6ES7151-1AA04-0AB0

X1)2)

-
IM151-1 STANDARD
as from 6ES7151-1AA05-0AB0
X1)2) X1)
IM151-1 FO
6ES7151-1AB02-0AB0
X1)2) -
IM151-1 FO
as from
6ES7151-1AB05-0AB0
X1)2) X1)
IM151-1 HIGH FEATURE
6ES7151-1BA01-0AB0
X1)2) -
IM151-1 HIGH FEATURE
as from 6ES7151-1BA02-0AB0
X1)2) X1)
IM151-3 PN STANDARD
as from 6ES7151-3AA23-0AB0
X2)3) X3)
IM151-3 PN HIGH FEATURE
as from 6ES7151-3BA23-0AB0
X2)3) X3)
IM151-3 PN FO
as from 6ES7151-3BB23-0AB0
X2)3) X3)
Table 01

1) For option handling you need one of the power modules below:

  • PM-E (DC24-48V/AC24-230V) as from 6ES7138-4CB10-0AB0
  • PM-E (DC24-48V) as from 6ES7138-4CA50-0AB0
  • PM-E (DC24V HF) as from 6ES7138-4CA60-0AB0

2) For option handling with reserve modules you need reserve modules as replacement for the future electronics modules:

  • Reserve module as from 6ES7138-4AA01-0AA0 (15mm)
  • Reserve module as from 6ES7138-4AA10-0AA0 (30mm)

3) The PROFINET IMs do not need any special power module for option handling, because the parameterization is cyclic by means of data records.

Note

  • With PROFIBUS it is important that both modules, the interface module and the power module, support option handling. If only one of these modules in your configuration supports the function, then you cannot configure option handling.
  • With PROFINET you can combine both processes, option handling with and without reserve modules. The "Retrofitting IO modules at the end of the station" function is also supported.
  • The IM151-7 CPU and the IM151-8 PN/DP CPU do not support option handling.

Additional information
Sample applications of option handling with ET 200 are available in Entry ID 29430270.

More information about option handling with and without Reserve modules is available in the following:

  • Operating manual "ET 200S Distributed IO System". The manual is available in Entry ID: 1144348 .
  • Manual for module IM151-1 HF in Entry ID: 25548028
  • Manual for module IM151-1 ST in Entry ID: 25548014
  • Manual for module IM151-3 PN ST in Entry ID: 30598131
  • Manual for module IM151-3 PN HF in Entry ID: 30609285
  • Manual for module IM151-3 PN FO in Entry ID: 36038272

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.