×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 22581930, Entry date: 01/27/2010
(0)
Rate

SIMATIC ET 200S FC: Application sample - FB100 - for diagnosis and set up via Touchpanel TP170B

  • Entry
  • Associated product(s)

Task:

This program example is based on the partner function block of the FB100 frequency converter (ET200S_FC_DRIV) and provides the following features:

  • Complete quick commissioning and optimization of one or several ET200S FC drives from a TP170B panel
  • Operator interface to operate the ET200S FC drive independently from other parts of your program
  • Diagnostic screen to read-out and acknowledge ET200S FC fault messages.
  • Screen to simply write to and read from the MMC parameter memory.

 

Solution:

You will learn about the individual FB100 functions step-by-step using several variable tables.

 

Exclusion:

When an ICU24F (safety ICU) is used, it isn’t possible to completely commission this via the TP170B screen. The reason for this is that it is not permissible to influence safety parameters using the Step 7 program.

The safety parameters still have to be entered using the “STARTER” commissioning tool.

 

 

Downloads

Content of Downloads

Download

Documentation
ET200S_FC_Shell_touchpanel_en_V_42.pdf
ET200S_FC_Shell_touchpanel_en_V_42.pdf ( 393 KB )
Code  FC_SHELL_E.zip ( 618 KB )

 

History

Version Date

Modification

V1.0 February 2005 First edition
V1.1 January 2006 Document reviewed
V1.2 February 2006 HTML-page added, document reviewed
V1.3 August 2006 Document reviewed
V1.4 October 2006 Program added

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.