Entry type: FAQ, Entry ID: 22632919, Entry date: 07/02/2007
(0)
Rate

How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?

  • Entry
  • Associated product(s)

Instruction:
Proceed as follows in STEP 7 Micro/WIN to activate multimaster mode in the network.
 

Step Procedure
1 Make sure that the navigation bar is visible in STEP 7 Micro/WIN (menu "View/Frame/Navigation Bar").
2 Click on the "Set PG/PC interface" button.
3 Select the PPI interface used and click on "Properties".
4 In the "PPI" tab enable the check box for "Multimaster network" and close the Properties window by clicking "OK" twice.

Note:
The following cables are multimaster-compatible: 
 

Product MLFB
Intelligent RS232/PPI cable with built-in RS232/RS485 converter 6ES7 901-3CB30-0XA0
Intelligent USB/PPI cable with built-in USB/RS485 converter 6ES7 901-3DB30-0XA0

Keywords:
Multimaster mode, PPI, Interface

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster