Entry type: FAQ, Entry ID: 22642255, Entry date: 03/07/2006
(0)
Rate

How do you block a user account after a user-definable number of failed attempts to login?

  • Entry
  • Associated product(s)

Description:
Since SIMATIC Logon operates with Microsoft Windows users, this operating system's security guidelines are used. If a user logs on locally, these settings have to be configured on each computer. If SIMATIC Logon is used to logon on a central logon computer, the settings only have to be defined there.

In order to set up an account blocking threshold, define the following setting under "Start > Settings > Control Panel > Administrative Tools > Local security guideline".


SIMATIC Logon also works after this with these settings.

Note:
Besides activating an account block, the settings for the "Account block duration" and "Reset duration for the account-block counter" may also be useful. This way, the administrator doesn't have to unblock the account each time there are x failed attempts. However, given the set delays, the system is still secure.
 

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster