×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 22950568, Entry date: 04/27/2006
(0)
Rate

Why are operator messages shown only on the OS server and not on the OS client?

  • Entry
  • Associated product(s)

Description:
In the case of a system with a client-server structure problems might arise on individual stations if their system times are different. One sort of behavior that often occurs is that no operator messages are shown on the OS clients. Please make sure that all stations of the PCS 7 system have the identical time. To ensure that this requirement is fulfilled you can use the PCS 7 time-of-day synchronization. There is further information available under Entry ID: 16622902.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.