×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 22957223, Entry date: 12/16/2004
(1)
Rate

Read / write global NC user data (GUDs) from the PLC.

  • Entry
  • Associated product(s)

DESCRIPTION:
Read / write global NC user data (GUDs) from the PLC.GUDs can be read via FB5.

A token is generated which is used to read/write the respective user data via FB3/2. In the example attached (S7 source), GUDs of the string and real types are being read and written.

Software:

  FB5_GUD.zip ( 2 KB )   

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.