How do you switch an operator panel to transfer mode when the autostart's timeout is set to 0 seconds?
-
Entry
-
Associated product(s)
Instructions:
No. | Procedure |
1 | If "Zero Seconds" is set for the delay time ("Autostart" or "Startup Delay") when the operator panel is started, then the operator panel starts with the corresponding Runtime configuration directly after booting.
|
2 | If you wish to make settings afterwards in the Control Panel or wish to enable the Transfer mode directly on the operator panel, then you must configure the "Stop Runtime" function or "Open Control Panel" function in your configuration.
|
3 | Below we take an MP 370 Touch to demonstrate how to proceed when the autostart is set to zero seconds and no "Stop Runtime" function or "Open Control Panel" function is configured.
Note: If a transfer is to be triggered by a configuration computer, under the following conditions there can be no automatic switch to Transfer mode (from the running operation):
|
4 | Remedy: There is the following option for switching the panel into transfer mode for the project download. Using the ProSave software you can reset the operator panel back to its factory settings (booting). Note: Cable: Refer to the relevant manual to see which interface your panel supports. *) Refer to the note in Step 5 |
5 | Note on the MP 377 Touch/Key With MP 377, to be able to select the "Reset to factory settings" function you must specify Ethernet in the menu "General > Connection" and an IP address under "Connection parameters". |
6 | Executing the "Reset to factory settings" function: A detailed description and instructions for executing the ""Reset to factory settings" function are available in the Entry ID 19701610 and in the relevant device manual. |
- German
- French
- Italian
- Spanish
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC PLC SIMATIC C7 Control systems
- Automation Technology Operator control and monitoring systems Operator devices Advanced HMI Panel-based Mobile Panels Mobile Panels Series x70 SIMATIC Mobile Panel 170
- Automation Technology Operator control and monitoring systems Operator devices Advanced HMI Panel-based Mobile Panels Mobile Panels Series x70 SIMATIC Mobile Panel 177
- Automation Technology Operator control and monitoring systems Operator devices Advanced HMI Panel-based Mobile Panels Mobile Panels Series x70 SIMATIC Mobile Panel 277
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Micro Panels SIMATIC OP 73micro
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Micro Panels SIMATIC TP 170micro
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Micro Panels SIMATIC TP 177micro
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Panels series 70 SIMATIC OP 73
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Panels series 70 SIMATIC OP 77A
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Panels series 70 SIMATIC OP 77B
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Panels Series 170
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Panels Series 270
- Automation Technology Operator control and monitoring systems Operator devices Previous systems Multi Panels Series 270
- Automation Technology Operator control and monitoring systems Archive SIMATIC HMI Panels 070/170/270 Panels
- Automation Technology Operator control and monitoring systems Archive SIMATIC HMI Panels Multi Panels
- Automation Technology Operator control and monitoring systems Archive SIMATIC Panel PC SIMATIC Panel PC IL 70
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC 577
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC 677
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC 877
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC 670
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC 870
- Automation Technology PC-based Automation SIMATIC Industrial PC Panel PC SIMATIC Panel PC IL 77