×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 23036220, Entry date: 12/15/2004
(2)
Rate

Preselect/start asynchronous subprogram (ASUP) via PLC.

  • Entry
  • Associated product(s)

DESCRIPTION:

An ASUP to be started must be assigned to an interrupt via FB4. It can then be started for specific channels by setting the interrupt via FC9.

In the PLC program attached (FB58), up to eight ASUPS are assigned to the interrupts 1 to 8 (Default: Asup1.spf to Asup8.spf  as user cycles – the program name can be changed in the Instance DB of the FB58). One ASUP each can be started in  channel 1 and channel 2 by entering the interrupt no.

The download file comprises the corresponding PLC blocks (in source format resp. as archived S7 project with 8xd-GP6.4) and NC data (NC archive for simulator and ASUP programs.).

Software:

  Asup_PLC.zip ( 245 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.