×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 23050125, Entry date: 04/24/2006
(0)
Rate

DriveMonitor, reference list entries in the "Drive properties" screen and order numbers.

  • Entry
  • Associated product(s)
QUESTION:
I’ve bought a MASTERDRIVES unit, order no. 6SE7016 - 1TA61 and wish to go online with the DriveMonitor.Which device type has to be selected in the "Drive properties" screen ?

ANSWER:
The attached table "DriveMonitor_MLFB.pdf" is a reference list containing the entries made in the "Drive properties" screen of the DriveMonitor and the relevant order numbers. The order numbers defining the relevant unit are marked in bold.Note: This reference list only includes MASTERDRIVES units.
KHED1382_4424_6464_DriveMonitor_MLFB.pdf ( 14 KB )
Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.