×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 23061262, Entry date: 03/31/2017
(2)
Rate

How do you set up Autostart for WinCC?

  • Entry
  • Associated product(s)
You can use the "Autostart" function to start WinCC with a specific project when the computer starts up.

There are two different ways of setting a WinCC Autostart. Either you use the WinCC tool "AutoStart Configuration" or the Autostart is written with the "AutoStartRT" tool into the communication setting of SIMATIC NET.

Depending on the version and operating mode of WinCCalways use only one of the two methods for configuring WinCC Autostart:

Use the "Autostart Configuration" tool without SIMATIC NET

  • WinCC V7.4 and higher (PCS 7 V8.2)
  • If you want to operate a WinCC project in the Service Mode (possible with WinCC V7.0 and higher)
  • In conjunction with SIMATIC NET (up to and including CD11/2003 SP1

Use the "AutoStartRT" tool with SIMATIC NET

  • WinCC V6.0 SP3 and higher (SIMATIC NET Edition 2005 and higher) to WinCC V7.3

Note

For synchronization problems refer also to Entry ID 19249315.
  

Set up Autostart with the "Autostart Configuration" tool without SIMATIC NET

Information about this is available in the WinCC Online Help and the associated manuals in this path:

"Working with WinCC > Working with Projects > Enable Project > How to set up AutoStart".

VersionTopic
WinCC V7.4 SP1How to set up Autostart for V7.4 SP1
WinCC V7.4

How to set up Autostart for V7.4

WinCC V7.3

How to set up AutoStart for V7.3

WinCC V7.2

How to set up AutoStart for V7.2

WinCC V7.0

How to set up AutoStart for V7.0


Set up Autostart with the "Autostart Configuration" tool without SIMATIC NET in the WinCC Service Mode

Proceed as under "Set up Autostart with the "Autostart Configuration" tool without SIMATIC NET".

In Service Mode the only difference is the operating mode of WinCC:

  • On the server, the project is operated in WinCC Service Mode as Service Project.
  • The automatic start is executed without an interactive user being logged on.
  • The Service Project is activated automatically as soon as the server starts up. User inputs are not required.
  • WinCC Runtime starts as a service.

Further information about this is available in the WinCC Online Help and the associated manuals:

WinCC Service Mode
How to Activate a Service Project
How to Define a Project as a Service Project

Note

After converting the Service Project to a Standard Project and vice versa you have to set up the "Autostart Configuration" again.

Set up Autostart with the "Autostart Configuration" tool with SIMATIC NET

  1. Open "Set Configuration Console PC Station" via the Windows Start menu.

    For Microsoft Windows 7 / Server 2008:
    "START > All Programs > Siemens Automation > SIMATIC > SIMATIC NET > Communication Settings" or
    "START > All Programs > Siemens Automation > SIMATIC > SIMATIC NET > Set PC Station"

    For Microsoft Windows XP:
    "START > SIMATIC > SIMATIC NET > Set PC Station"

    For Microsoft Windows Server 2003:
    "START > SIMATIC > SIMATIC NET > Configuration Console" or
    "START > SIMATIC > SIMATIC NET > Set PC Station"

  2. Open the dialog "SIMATIC NET Configuration > Autostart" or

    In the "Set Configuration Console PC Station" dialog, you open the dialog for AutoStart configuration through "PC Station > SIMATIC NET Configuration > Applications > AutoStart"
     


    Fig. 01

  3. Click the the "New" button to insert a new application that is to be started automatically. A dialog opens in which you select and apply the WinCC application "<SIEMENS Installation Path> SIEMENS > WinCC > bin > AutoStartRT.exe".

  4. In the "Call parameters" input field you enter the parameters for the WinCC application "AutoStartRT.exe" (Step 2 - Fig. 01). Use the following syntax:

    <Drive>:\<Project path>\<Project name>.mcp /Active:yes /LANG=ENU /EnableBreak:no

    Note
    The first parameter "<Drive>:\<Project path>\<Project name>.mcp" gives the complete path for the WinCC project to be started.

    With the/Active parameter you decide whether the project is to be opened only in WinCC Runtime or whether the WinCC project is to be opened briefly and then closed again immediately.

    • /Active:yes
      The WinCC project is opened only in WinCC Runtime. The WinCC Explorer is not started.
    • /Active:no
      The WinCC project is opened briefly in the WinCC Explorer and then closed again immediately.

    With the /LANG parameter you preselect the language for display of the "AutoStartRT" tool.

    • /LANG=DEU
      Runtime language is German
    • /LANG=ENU
      Runtime language is English

    With the /EnableBreak parameter you enable/disable the "Cancel" button.

    • /EnableBreak:no
      It is not possible to operate the "Cancel" button while "AutoStartRT" is being executed.
    • /EnableBreak:yes
      It is possible to operate the "Cancel" button while "AutoStartRT" is being executed.

  5. Save the settings with the "Apply" button (Step 2 - Fig. 01). The next time the system is started up the WinCC tool "AutoStartRT" will be executed with the settings chosen.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.