×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 2334224, Entry date: 06/12/2015
(10)
Rate

With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible?

  • Entry
  • Associated product(s)
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

Compatibility information for PCS 7 is available in the Compatibility Tool.
You can call the Compatibility Tool in the following entry.
64847781

Please use the new entry for your favorites.

This entry also includes the following information:

  • New compatibility information
  • New Compatibility Tool functions
  • Operating instructions and Help for the Compatibility Tool
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.