×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 23510608, Entry date: 06/13/2006
(1)
Rate

OMC TP11 and OMC TP11-LD Media Converters to Be Phased Out

  • Entry
  • Associated product(s)

The OMC TP11 and OMC TP11-LD optical media converters will be declared mature products as per October 01, 2006. This means that the products will remain available for normal ordering for the time being, but should not be used for new projects anymore.

 

 

The products listed below will be declared mature products as per October 01, 2006 and their list price will be increased. The modules will remain available for normal ordering until September 30, 2007. As per October 01, 2007 the products will be given spare part status and remain available on this basis for another 9 years.

The following products are affected by the phaseout:

Product Designation

Order No.

OMC TP11

6GK1 100-2AB00

OMC TP11-LD

6GK1 100-2AC00

The following products are available for direct replacement:

Product Designation

Order No.

SCALANCE X101-1
has one electrical 10/100 MBit/s RJ45 port and one 100 Mbit/s Multimode interface with BFOC connector.

6GK5101-1BB00-2AA3

SCALANCE X101-1LD
has one electrical 10/100 MBit/s RJ45 port and one 100 Mbit/s Single-mode interface with BFOC connector.

6GK5101-1BC00-2AA3

 

More information on these products is available under entry ID:  !22476584!

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.