Entry type: FAQ, Entry ID: 23578647, Entry date: 07/05/2006
(0)
Rate

Is there any way of configuring an ET 200 multi-tiered?

  • Entry
  • Associated product(s)

 
Configuration Notes:
Current ET 200 stations do not support multi-tiered setups such as were possible with the ET 200U, for example.
ET 200Ms can also only be configured with a single tier because connection to other module racks via interface modules is not permissible.

If the maximum configuration of the ET 200 station is inadequate, a further ET 200 station must be added to the PROFIBUS.

Keywords:
ET 200S, ET 200iSP, ET 200iS, ET 200pro, ET 200X, ET 200L, ET 200M, ET 200B, ET 200eco, ET 200R, IM 360, IM 361, IM 365, Single tier, Multi-tier, Setup, Maximum configuration, Mounting channel, Module rack