Entry type: FAQ, Entry ID: 23678970, Entry date: 01/20/2016
(5)
Rate

Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?

  • Entry
  • Associated product(s)
With the extended PROFINET diagnostics it is possible to have functions like the diagnostics and parameterization of integrated Ethernet interfaces (fiber-optic diagnostics and topology configuration, for example).

The PROFINET IO devices that support extended PROFINET diagnostics are configured in the STEP 7 Hardware Configuration. They are available in the hardware catalog and have additional ports or interface modules as subslots in the module's slot. 

More information about PROFINET diagnostics and how to implement the PROFINET device module in SIMATIC is available in the manual "SIMATIC PROFINET with STEP 7 V13" in Entry ID 49948856.

Example
ET200S with extended PROFINET diagnostics
 

Fig. 01

The following IO controllers support the extended PROFINET diagnostics
 
 

ModuleArticle numberFirmware
SIMATIC NET PC-Software / PN-Treiber
CP 16166GK1161-6AA02
6GK1161-6AA01
6GK1161-6AA00
from V2.0
CP 16046GK1160-4AA02
6GK1160-4AA01
6GK1160-4AA00
from V2.0
SOFTNET PROFINET IO6GK1704-1HW71-3AA0from V7.1 (Edition 2008)
Embedded und PC-based Automation
WinAC RTX 20086ES7671-0RC06-0YA0V4.4
WinAC RTX (F) 20096ES7671-0RC07-0YA0
6ES7671-1RC07-0YA0
V4.5
WinAC RTX (F) 20106ES7671-0RC08-0YA0
6ES7671-1RC08-0YA0
V4.6
S7-mEC, EC31-RTX6ES7677-1DD00-0BB0
6ES7677-1DD10-0BB0
from V4.4
S7-400 CPUs
CPU 410-5H 6ES7410-5HX08-0AB0 from V8.0 
CPU 412-2 PN6ES7412-2EK06-0AB0from V6.0
CPU 412-2 PN 6ES7412-2EK07-0AB0 from V7.0 
CPU 414-3 PN/DP6ES7414-3EM05-0AB0from V5.0
CPU 414-3 PN/DP6ES7414-3EM06-0AB0from V6.0
CPU 414-3 PN/DP 6ES7414-3EM07-0AB0 from V7.0 
CPU 414F-3 PN/DP6ES7414-3FM06-0AB0from V6.0
CPU 414F-3 PN/DP 6ES7 414-3FM07-0AB0 from V7.0 
CPU 416-3 PN/DP6ES7416-3ER05-0AB0from V5.0
CPU 416-3 PN/DP6ES7416-3ES06-0AB0from V6.0
CPU 416-3 PN/DP 6ES7416-3ES07-0AB0  from V7.0 
CPU 416F-3 PN/DP6ES7416-3FR05-0AB0from V5.0
CPU 416F-3 PN/DP6ES7416-3FS06-0AB0from V6.0
CPU 416F-3 PN/DP 6ES7416-3FS07-0AB0 from V7.0 
CPU 412-5H PN/DP6ES7412-5HK06-0AB0from V6.0
CPU 414-5H PN/DP6ES7414-5HM06-0AB0from V6.0
CPU 416-5H PN/DP6ES7416-5HS06-0AB0
from V6.0
CPU 417-5H PN/DP6ES7417-5HT06-0AB0from V6.0
S7-300 CPUs
CPU 314C-2 PN/DP
6ES7314-6EH04-0AB0
from V3.3
CPU 315-2 PN/DP6ES7315-2EH13-0AB0from V2.5
CPU 315-2 PN/DP6ES7315-2EH14-0AB0from V3.1
CPU 315F-2 PN/DP6ES7315-2FH13-0AB0from V2.5
CPU 315F-2 PN/DP6ES7315-2FJ14-0AB0from V3.1
CPU 315T-3 PN/DP6ES7315-7TJ10-0AB0from V3.2
CPU 317-2 PN/DP6ES7317-2EK13-0AB0from V2.5
CPU 317-2 PN/DP6ES7317-2EK14-0AB0from V3.1
CPU 317F-2 PN/DP6ES7317-2FK13-0AB0from V2.5
CPU 317F-2 PN/DP6ES7317-2FK14-0AB0from V3.1
CPU 317T-3 PN/DP6ES7317-7TK10-0AB0from V3.2
CPU 317TF-3 PN/DP
6ES7317-7UL10-0AB0
from V3.2
CPU 319-3 PN/DP6ES7318-3EL00-0AB0from V2.5
CPU 319-3 PN/DP6ES7318-3EL01-0AB0from V3.2
CPU 319F-3 PN/DP6ES7318-3FL00-0AB0from V2.5
CPU 319F-3 PN/DP6ES7318-3FL01-0AB0from V3.2
S7-1500 CPUs
CPU 1518-4 PN/DP6ES7518-4AP00-0AB0from V1.5
CPU 1518F-4 PN/DP6ES7518-4FP00-0AB0from V1.5
CPU 1517-3 PN/DP6ES7517-3AP00-0AB0from V1.6
CPU 1517F-3 PN/DP6ES7517-3FP00-0AB0from V1.6
CPU 1516-3 PN/DP6ES7516-3AN01-0AB0from V1.8
CPU 1516-3 PN/DP6ES7516-3AN00-0AB0from V1.0
CPU 1516F-3 PN/DP6ES7516-3FN01-0AB0from V1.8
CPU 1516F-3 PN/DP6ES7516-3FN00-0AB0from V1.5
CPU 1515-2 PN/DP6ES7515-2AM01-0AB0from V1.8
CPU 1515-2 PN6ES7515-2AM00-0AB0from V1.5
CPU 1515F-2 PN6ES7515-2FM01-0AB0from V1.8
CPU 1515F-2 PN6ES7515-2FM00-0AB0from V1.6
CPU 1513-1 PN6ES7513-1AL01-0AB0from V1.8
CPU 1513-1 PN6ES7513-1AL00-0AB0from V1.0
CPU 1513F-1 PN6ES7513-1AL01-0AB0from V1.8
CPU 1513F-1 PN6ES7513-1FL00-0AB0from V1.7
CPU 1511-1 PN6ES7511-1AK01-0AB0from V1.8
CPU 1511-1 PN6ES7511-1AK00-0AB0from V1.0
CPU 1511F-1 PN6ES7511-1FK01-0AB0from V1.8
CPU 1511F-1 PN6ES7511-1FK00-0AB0from V1.7
CPU 1511C-1 PN6ES7511-1CK00-0AB0from V1.8
CPU 1512C-1 PN6ES7512-1CK00-0AB0from V1.8
ET 200SP CPUs
CPU 1510SP-1 PN6ES7510-1DJ01-0AB0from V1.8
CPU 1510SP-1 PN6ES7510-1DJ00-0AB0from V1.6
CPU 1510SP F-1 PN6ES7510-1SJ01-0AB0from V1.8
CPU 1510SP F-1 PN6ES7510-1SJ00-0AB0from V1.7
CPU 1512SP-1 PN6ES7512-1DK01-0AB0from V1.8
CPU 1512SP-1 PN6ES7512-1DK00-0AB0from V1.6
CPU 1512SP F-1 PN6ES7512-1SK01-0AB0from V1.8
CPU 1512SP F-1 PN6ES7512-1SK00-0AB0from V1.7
S7-1500 Software Controllers
CPU 1507S6ES7672-7AC00-0YA0from V1.8
CPU 1505S6ES7672-5AC00-0YA0from V1.7
S7-1200 CPUs
CPU 1211C6ES7211-1AD30-0XB0
6ES7211-1BD30-0XB0
6ES7211-1HD30-0XB0
from V1.0
6ES7211-1AE31-0XB0
6ES7211-1BE31-0XB0
6ES7211-1HE31-0XB0
from V3.0
6ES7211-1AE40-0XB0
6ES7211-1BE40-0XB0
6ES7211-1HE40-0XB0
from V4.0
CPU 1212C6ES7212-1AD30-0XB0
6ES7212-1BD30-0XB0
6ES7212-1HD30-0XB0
from V1.0
6ES7212-1AE31-0XB0
6ES7212-1BE31-0XB0
6ES7212-1HE31-0XB0
from V3.0
6ES7212-1AE40-0XB0
6ES7212-1BE40-0XB0
6ES7212-1HE40-0XB0
from V4.0
CPU 1214C6ES7214-1AE30-0XB0
6ES7214-1BE30-0XB0
6ES7214-1HE30-0XB0
from V1.0
6ES7214-1AG31-0XB0
6ES7214-1BG31-0XB0
6ES7214-1HG31-0XB0
from V3.0
6ES7214-1AG40-0XB0
6ES7214-1BG40-0XB0
6ES7214-1HG40-0XB0
from V4.0
CPU 1215C6ES7215-1AG31-0XB0
6ES7215-1BG31-0XB0
6ES7215-1HG31-0XB0
from V3.0
6ES7215-1AG40-0XB0
6ES7215-1BG40-0XB0
6ES7215-1HG40-0XB0
from V4.0
CPU 1217C6ES7217-1AG40-0XB0from V4.0
Industrial Ethernet CPs S7-300/S7-400
CP343-1 Standard6GK7343-1EX30-0XE0from V2.2
CP343-1 Advanced6GK7343-1GX30-0XE0from V1.0
CP343-1 Advanced6GK7343-1GX31-0XE0from V3.0
CP443-1 Standard6GK7443-1EX20-0XE0from V1.0
CP443-1 Standard6GK7443-1EX30-0XE0from V3.0
CP443-1 Advanced6GK7443-1GX20-0XE0from V2.0
CP443-1 Advanced6GK7443-1GX30-0XE0from V3.0
Industrial Ethernet CMs
CM 1242-16GK7542-1AX00-0XE0from V1.0
ET 200S
IM151-8 PN/DP CPU6ES7151-8AB00-0AB0from V2.7
IM151-8 PN/DP CPU6ES7151-8AB01-0AB0from V3.2
IM151-8F PN/DP CPU6ES7151-8FB00-0AB0from V2.7
IM151-8F PN/DP CPU6ES7151-8FB01-0AB0from V3.2
ET 200pro
IM154-8 CPU6ES7154-8AB00-0AB0from V2.5
IM154-8 CPU6ES7154-8AB01-0AB0from V3.2
IM154-8F CPU6ES7154-8FB01-0AB0from V3.2
IM154-8FX CPU6ES7154-8FX00-0AB0from V3.2

Table 1

The IO devices below support extended PROFINET diagnostics
   

ModuleArticle numberFirmware
PC CPs
CP16166GK1161-6AA02
6GK1161-6AA01
6GK1161-6AA00
from V2.0
CP16046GK1160-4AA02
6GK1160-4AA01
6GK1160-4AA00
from V2.0
S7-300 CPUs
CPU 314C-2 PN/DP
6ES7314-6EH04-0AB0
from V3.3
CPU 315-2 PN/DP6ES7315-2EH14-0AB0from V3.2
CPU 315F-2PN/DP6ES7315-2FJ14-0AB0from V3.2
CPU 315T-3 PN/DP6ES7315-7TJ10-0AB0from V3.2
CPU 317-2 PN/DP6ES7317-2EK14-0AB0from V3.2
CPU 317F-2PN/DP6ES7317-2FK14-0AB0from V3.2
CPU 317T-3 PN/DP6ES7317-7TK10-0AB0from V3.2
CPU 317TF-3 PN/DP6ES7317-7UL10-0AB0from V3.2
CPU319-3 PN/DP6ES7318-3EL01-0AB0from V3.2
CPU319F-3 PN/DP6ES7318-3FL01-0AB0from V3.2
S7-400 CPUs
CPU 412-2 PN6ES7412-2EK06-0AB0from V6.0
CPU 412-2 PN 6ES7412-2EK07-0AB0  from V7.0 
CPU 414-3 PN/DP 6ES7414-3EM05-0AB0 from V5.0 
CPU 414-3 PN/DP6ES7414-3EM06-0AB0from V6.0
CPU 414-3 PN/DP 6ES7414-3EM07-0AB0 from V7.0 
CPU 414F-3 PN/DP6ES7414-3FM06-0AB0from V6.0
CPU 414F-3 PN/DP 6ES7414-3FM07-0AB0 from V7.0 
CPU 416-3 PN/DP 6ES7416-3ER05-0AB0 from V5.0 
CPU 416-3 PN/DP6ES7416-3ES06-0AB0from V6.0
CPU 416-3 PN/DP 6ES7416-3ES07-0AB0 from V7.0 
CPU 416F-3 PN/DP 6ES7416-3FR05-0AB0 from V5.0 
CPU 416F-3 PN/DP6ES7416-3FS06-0AB0from V6.0
CPU 416F-3 PN/DP 6ES7416-3FS07-0AB0 from V7.0 
S7-1500 CPUs
CPU 1518-4 PN/DP6ES7518-4AP00-0AB0from V1.5
CPU 1518F-4 PN/DP6ES7518-4FP00-0AB0from V1.5
CPU 1517-3 PN/DP6ES7517-3AP00-0AB0from V1.6
CPU 1517F-3 PN/DP6ES7517-3FP00-0AB0from V1.6
CPU 1516-3 PN/DP6ES7516-3AN01-0AB0from V1.8
CPU 1516-3 PN/DP6ES7516-3AN00-0AB0from V1.0
CPU 1516F-3 PN/DP6ES7516-3FN01-0AB0from V1.8
CPU 1516F-3 PN/DP6ES7516-3FN00-0AB0from V1.5
CPU 1515-2 PN6ES7515-2AM01-0AB0from V1.8
CPU 1515-2 PN6ES7515-2AM00-0AB0from V1.5
CPU 1515F-2 PN6ES7515-2FM01-0AB0from V1.8
CPU 1515F-2 PN6ES7515-2FM00-0AB0from V1.6
CPU 1513-1 PN6ES7513-1AL01-0AB0from V1.8
CPU 1513-1 PN6ES7513-1AL00-0AB0from V1.0
CPU 1513F-1 PN6ES7513-1FL01-0AB0from V1.8
CPU 1513F-1 PN6ES7513-1FL00-0AB0from V1.7
CPU 1511-1 PN6ES7511-1AK01-0AB0from V1.8
CPU 1511-1 PN6ES7511-1AK00-0AB0from V1.0
CPU 15111F-1 PN6ES7511-1FK01-0AB0from V1.8
CPU 15111F-1 PN6ES7511-1FK00-0AB0from V1.7
CPU 1511C-1 PN6ES7511-1CK00-0AB0from V1.8
CPU 1512C-1 PN6ES7512-1CK00-0AB0from V1.8
ET 200SP CPUs
CPU 1510SP-1 PN6ES7510-1DJ01-0AB0from V1.8
CPU 1510SP-1 PN6ES7510-1DJ00-0AB0from V1.6
CPU 1510SP F-1 PN6ES7510-1SJ01-0AB0from V1.8
CPU 1510SP F-1 PN6ES7510-1SJ00-0AB0from V1.7
CPU 1512SP-1 PN6ES7512-1DK01-0AB0from V1.8
CPU 1512SP-1 PN6ES7512-1DK00-0AB0from V1.6
CPU 1512SP F-1 PN6ES7512-1SK01-0AB0from V1.8
CPU 1512SP F-1 PN6ES7512-1SK00-0AB0from V1.7
S7-1500 Software Controllers
CPU 1507S6ES7672-7AC00-0YA0from V1.8
CPU 1505S6ES7672-5AC00-0YA0from V1.7
Industrial Ethernet CPs S7-300/S7-400
CP343-1 Lean6GK7343-1CX10-0XE0from V2.2
CP343-1 Standard6GK7343-1EX30-0XE0from V2.2
CP343-1 Advanced6GK7343-1GX30-0XE0from V1.0
CP343-1 Advanced6GK7343-1GX31-0XE0from V3.0
ET 200SP
IM 155-6 PN ST6ES7155-6AU00-0BN0V1.0 and higher
IM 155-6PN HF6ES7155-6AU00-0CN0V2.0 and higher
ET 200MP
IM 155-5 PN ST6ES755-5AA00-0AB0V1.0 and higher
IM 155-5 PN HF6ES755-5AA00-0AC0V1.0 and higher
ET 200AL
IM 157-1 PN6ES7157-1AB00-0AB0from V1.0
ET 200S
IM151-3PN FO6ES7151-3BB21-0AB0 and higherfrom V4.0
IM151-3PN ST6ES7151-3AA20-0AB0 and higherfrom V4.0
IM151-3PN HF6ES7151-3BA20-0AB0 and higherfrom V4.0
IM151-3PN HS6ES7151-3BA50-0AB0 and higherfrom V1.0
IM151-8 PN/DP CPU6ES7151-8AB01-0AB0from V3.2
IM151-8F PN/DP CPU6ES7151-8FB01-0AB0from V3.2
ET 200M
IM153-4PN6ES7153-4AA00-0XB0from V1.0
IM153-4PN6ES7153-4AA01-0XB0from V2.0
ET 200pro
IM154-4PN HFV2.0 and higherfrom 6ES7154-4AB00-0AB0
IM154-8 CPUV3.2 and higher6ES7154-8AB01-0AB0
IM154-8F CPUV3.2 and higher6ES7154-8FB01-0AB0
IM154-8FX CPUV3.2 and higher6ES7154-8FX00-0AB0
ET 200eco PN
ET 200eco PNV6.0 and higher

6ES7141-6BF00-0AB0
6ES7141-6BG00-0AB0
6ES7141-6BH00-0AB0
6ES7142-6BF00-0AB0
6ES7142-6BF50-0AB0
6ES7142-6BG00-0AB0
6ES7142-6BH00-0AB0
6ES7142-6BR00-0AB0
6ES7144-6KD00-0AB0
6ES7145-6HD00-0AB0
6ES7147-6BG00-0AB0
6ES7144-6KD50-0AB0
6ES7148-6JA00-0AB0

Network components
PN/PN couplerV1.0 and higher6ES7158-3AD00-0XA0
SCALANCE X20x IRT productsV2.1 and higher-
SCALANCE X200 productsV2.1 and higher

-
see Entry ID: 25472849

SCALANCE X300 productsV2.1 and higher-
SCALANCE X414-3 EV2.1.1 and higher

-
see Entry ID: 25355654

SCALANCE X408-2V2.0 and higher-
SCALANCE XM408-4CV5.0 and higher-
SCALANCE XM408-8CV4.1 and higher-
SCALANCE XM416-4CV4.1 and higher-
SCALANCE X500 productsV3.0 and higher-
Gateways
IE/AS Interface Link PN/IOV2.0 and higherSingle AS-i Master:
6GK1 411-2AB10

Double AS-i Master:
6GK1 411-2AB20

Table 2

The PROFINET IO devices that support the extended PROFINET diagnostics can only be operated on PROFINET IO controllers that likewise support the extended PROFINET diagnostics.

There is a migration GSDML file for some of the PROFINET IO devices listed above for operating the PROFINET IO device on a PROFINET IO controller that does not yet support the extended PROFINET diagnostics.

Example
PN/PN coupler
   


Fig. 02

Note
The following applications provide a detailed description, including sample program, of the diagnostics options available in a PROFINET IO system.

  • "Diagnostic Methods for PROFINET Network Components (PROFINET IO, SNMP, WBM)" in Entry ID: 21566216
  • "PROFINET IO – Diagnostics Processing in the User Program"
    In Entry ID: 24000238