×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 23678970, Entry date: 01/20/2016
(5)
Rate

Which PROFINET nodes support the extended PROFINET diagnostics and what do you have to configure?

  • Entry
  • Associated product(s)
With the extended PROFINET diagnostics it is possible to have functions like the diagnostics and parameterization of integrated Ethernet interfaces (fiber-optic diagnostics and topology configuration, for example).

The PROFINET IO devices that support extended PROFINET diagnostics are configured in the STEP 7 Hardware Configuration. They are available in the hardware catalog and have additional ports or interface modules as subslots in the module's slot. 

More information about PROFINET diagnostics and how to implement the PROFINET device module in SIMATIC is available in the manual "SIMATIC PROFINET with STEP 7 V13" in Entry ID 49948856.

Example
ET200S with extended PROFINET diagnostics
 

Fig. 01

The following IO controllers support the extended PROFINET diagnostics.

  23678970_IO_Controller_List_en.pdf (10,2 KB)

The IO devices below support extended PROFINET diagnostics.

  23678970_IO_Device_List_en.pdf (10,1 KB)

The PROFINET IO devices that support the extended PROFINET diagnostics can only be operated on PROFINET IO controllers that likewise support the extended PROFINET diagnostics.

There is a migration GSDML file for some of the PROFINET IO devices listed above for operating the PROFINET IO device on a PROFINET IO controller that does not yet support the extended PROFINET diagnostics.

Example
PN/PN coupler
   


Fig. 02

Note
The following applications provide a detailed description, including sample program, of the diagnostics options available in a PROFINET IO system.

  • "Diagnostic Methods for PROFINET Network Components (PROFINET IO, SNMP, WBM)" in Entry ID: 21566216
  • "PROFINET IO – Diagnostics Processing in the User Program"
    In Entry ID: 24000238

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
mySupport Cockpit
Related links