×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 23772935, Entry date: 10/13/2006
(0)
Rate

SINUMERIK 880, PLC-EPROM module, programming numbers.

  • Entry
  • Associated product(s)
QUESTION:
What are the programming numbers of the PLC-EPROM modules for the PLC 135WB?
These modules are not included in the list that is saved in the SIMATIC S5 software.

ANSWER:
The PLC 135WB (6FX1138-6BA01/-6BB01/-6BL01/-6BK01) can identify two different EPROM modules for the PLC user program.

Module 6FX1130-5BB00/-5BB10 (64KB) = programming number 162

Module 6FX1145-8BA00/-8BA10 (256KB) = programming number 129
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit