×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 23785345, Entry date: 09/21/2006
(0)
Rate

Multiproject Engineering with SIMATIC BATCH

  • Entry
  • Associated product(s)
Basic requirements and typical procedures with step-by-step instructions for multiproject engineering with SIMATIC BATCH.

Building on the instructions “Multiproject Engineering“ (ID: 22258951), the particularities when dealing with projects containing batch functions are described.

Unlike the base document the subprojects extracted from the multiproject are included here into other multiprojects (MP of the decentralized engineering environments). At this the implemented batch functions must be treated separately.

For simplicity reasons, the following abbreviations are used in this document:

  • CMMP (Central Master Multiproject)
  • DMP   (Decentralized Multiproject)

Main contents
The document focuses on the following points:

  • Principle procedure and basic requirements
  • Activities when dividing and merging the individual subprojects

From a GMP (Good Manufacturing Practice) point of view, the document is meant to help communicating the correct procedure for multiproject engineering with SIMATIC BATCH to the respective project engineers.

Validity
This entry was created with SIMATIC PCS 7 V8.1 and SIMATIC PCS 7 BATCH V8.1, the procedure is valid for SIMATIC PCS 7 and SIMATIC BATCH from V6.1.

Documentation
  Multiproject Engineering with SIMATIC BATCH (2,6 MB)

Further Information
Manual - SIMATIC Process Control System PCS 7 SIMATIC BATCH V9.0 SP1
Application example - PCS 7 Multiproject / Multiuser Engineering

History
Update of the validity

Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.