×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 23810112, Entry date: 05/30/2012
(1)
Rate

SINAUT ST7 Telecontrol configuration examples in Ethernet, secure Internet and (E)GPRS environment

  • Entry
  • Associated product(s)

Problem
A central station for controlling and monitoring remote Telecontrol stations shall be connected via a secure Internet/ (E)GPRS connection with two stations. A simple process (three motors) shall be operated and monitored via the central station as an example. The stations shall exchange process data in addition (cross-communication)

Solution
The automation solution uses the SINAUT ST7 Telecontrol System of SIMATIC NET. This telecontrol system is based on SIMATIC S7 and WinCC and permits

  • a fully automatic monitoring and visualization of the substations
  • an event-controlled data transmission through all networks
  • remote programming and diagnostics of the subordinated stations.

This document is divided into three partial configurations for the sake of clarity, to separate the purely SINAUT ST7-specific configurations from the configuration of the secure connection via IPSec or MSC protocol.

  • Volume 1: Application for SINAUT ST7 Telecontrol with TIM4R-IE and TIM3V-IE in an Ethernet-based environment
  • Volume 2: SINAUT ST7 Telecontrol configuration in a secure EGPRS environment with MD741-1/ SCALANCE S612
  • Volume 3: SINAUT ST7 Telecontrol configuration of a secure Internet/ GPRS connection via MSC protocol

Volume 1 shows the simplest option of connecting a central station and two SINAUT stations via Ethernet. For this purpose the WinCC station will have been connected with the ST7cc server via a Master TIM4R-IE with Industrial Ethernet. The stations are coupled with Industrial-Ethernet via a TIM3V-IE.


Fig. 01

This example gives a small overview over the topic "Telecontrol with SIMATIC" and explains in detail the configuration

  • of a SINAUT connection via Ethernet
  • of the signals from the CPU via the TIM3V-IE and ST7cc server into the WinCC tag management
    (Here the variant is demonstrated where the block library (TD7onTIM) is used which has already been integrated in TIM3V-IE)
  • of the SINAUT ST7 standard typicals within the WinCC surface

Volume 2 is based on this completed example, but here a secure EGPRS data transmission is used via the Internet instead of the line dependent connection. For this purpose the EGPRS router MD741-1 establishes a virtual private network (VPN) via the Internet to a SCALANCE S612 Security Module. A DSL line with a fixed IP address is used here for the Internet connection.


Fig. 02

This example explains

  • the necessary basic terms of the GSM/EGPRS technology and security aspects
  • all configuration steps in detail which are required to build a VPN tunnel between the EGPRS router MD741-1 and the security module SCALANCE S612

Volume 3 is based also on the completed example of Volume 1. In this example the MSC protocol is used for the secure data transmission via the Internet and GPRS. For this purpose the GSM/GPRS modem MD720-3 (or TIM3V-IE Advanced in a DSL station) builds a virtual private network (VPN) via the Internet to the Master TIM4R-IE without requiring any additional VPN devices. Like in Volume 2, a DSL line is used with a fixed IP address as Internet connection in the Control Center in this example.


Fig. 03

This example contains

  • information about the properties of the IE-TIM variants as of Firmware Version 2.0
  • all configuration steps which are required to build a VPN tunnel between the GSM/GPRS modem MD720-3 and the TIM4R-IE
  • all configuration steps which are required to build a VPN tunnel between the TIM3V-IE Advanced and the TIM4R-IE

Downloads

Content of Downloads

Download

Documentation Volume 1
Application for SINAUT ST7 Telecontrol with TIM4R-IE and TIM3V-IE in an Ethernet-based environment
23810112_SINAUT_LAN_DOKU_V20_e.pdf ( 4075 KB )
Code to Volume 1
WinCC/ST7cc-Projekt, STEP 7/SINAUT ST7 Programm
23810112_SINAUT_LAN_CODE_V20.zip ( 14297 KB )
Dokumentation Volume 2
SINAUT ST7 Telecontrol configuration in a secure EGPRS environment with MD741-1/ SCALANCE S612
23810112_SINAUT_INTERNET_DOKU_V23_e.pdf ( 1421 KB )
Code to Volume 2
WinCC/ST7cc-Projekt, STEP 7/SINAUT ST7 Programm
23810112_SINAUT_INTERNET_CODE_V20.zip ( 14332 KB )
Dokumentation Volume 3
SINAUT ST7 Telecontrol configuration of a secure Internet/ GPRS connection via MSC protocol
23810112_SINAUT_MSC_INTERNET_DOKU_e.pdf ( 1484 KB )
Code to Volume 3
WinCC/ST7cc-Projekt, STEP 7/SINAUT ST7 Programm
23810112_SINAUT_INTERNET_MSC_CODE.zip ( 9746 KB )
Flash animation to Volume 3
SINAUT ST7 Telecontrol instruction for the configuration of a secure Internet/ GPRS connection via MSC protocol, in form of a flash animation

Load the files to a folder which you select and unzip the animation. Start the animation with a double-click on the "exe" file which you unzipped from the archive.

Archives

Content of the archives

Archive version

Archive

If you use an MD740-1 GPRS router in your configuration, you can download the documentation for the configuration of the MD740-1 here (there are only Volume 1 and Volume 2 here).

 V1.0

23810112_Configuration_8_V1_0_e.zip ( 17786 KB )

Additional Information
The following application shows you a SINAUT solution using a dedicated line modem.

Title

Link

Communication Between S7-300 Stations by Using SINAUT ST7 Telecontrol via Dedicated Line and Ethernet Entry-ID: 48283510
Integration of Remote Terminal Units via DNP3 protocol in PCS 7 TeleControl Entry-ID: 60711573

Security Notice
Caution
The functions and solutions described in this article confine themselves to the realization of the automation task predominantly. Please take into account furthermore that corresponding protective measures have to be taken up in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the Internet. Further information can be found under the Content-ID 50203404.

Last Changes
Volume 2: Supplementation in chapter 5.3.7 (Table 5-18, Point 3), corrections in configuration, security configuration now with SCT V2.3

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.