×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 23849953, Entry date: 09/26/2006
(1)
Rate

Service Pack 1 for STEP 7 V5.4 and STEP 7 Professional Edition 2006

  • Entry
  • Associated product(s)

DESCRIPTION:

Download of Service Pack 1 for STEP 7 V5.4

Installation prerequisites:

  • STEP 7 V5.4
  • STEP 7 Professional Edition 2006 

Please also read the information (What’s NEW, special hints, etc.) we have compiled for you in entry ID 22445425.

Customers with a valid Software Update Service agreement for STEP 7 will receive the CD ROM with STEP 7 V5.4 incl. SP1 automatically.

Customers with a valid Software Update Service agreement for STEP 7 Professional will receive the CD ROM with the STEP 7 Professional Edition 2006 Service Release 1 automatically. The SP1 for STEP 7 V5.4 is part of this Professional CD (see entry ID 23848193 ).

Customers without Software Update Service agreement can obtain the SP1 as follows:

  1. Order the CD from LZN: You can order the Trial License with STEP 7 V5.4 incl. Service Pack 1.

    We are offering a Trial License with STEP 7 Professional Edition 2006 SR1 for the current STEP 7 Professional Edition 2006. This CD with the STEP 7 Professional Edition 2006 Service Release 1 includes the SP1 for STEP 7 V5.4
  2. Free Download
    As usual, we are offering a free download. However, please note the file sizes.

    Service Pack 1 for STEP 7 V5.4
    SIMATIC_S7_STEP7_V54_SP1.exe ( 194221 KB )

    This free download only includes the SP1 for STEP 7 V5.4 and NCM.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.