×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 23876782, Entry date: 11/10/2006
(0)
Rate

How can you replace the technology CPU already configured in a STEP 7 project with another technology CPU?

  • Entry
  • Associated product(s)

Instructions:
There is a specific procedure for replacing a configured technology CPU with another technology CPU. This entry contains a document that describes the procedure for replacing the technology CPU.

The attached document is divided as follows:

1 Backing up the Numbers of the Technology DBs
2 Upgrading the Configured CPU
    2.1 Replacing the CPU in HW Config
    2.2 Adapting the technology objects in S7T Config
    2.3 Regenerating the technology DBs in TOM
    2.4 Characteristic features when using the Microbox 420T
        2.4.1 Integrating the Microbox 420T
        2.4.2 Transferring the technology
        2.4.3 Transferring the PLC program
        2.4.4 Regenerating the technology DBs in TOM
        2.4.5 Final work
3 History

Attachment 1: T_CPU_Tausch_e.pdf ( 295 KB )

Keywords:
Change, Replacement

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.