×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 23995598, Entry date: 10/17/2006
(0)
Rate

Release for general availability, SinuCom commissioning and service tools SW release 7.2 (V07.02.00)

  • Entry
  • Associated product(s)

The SinuCom commissioning and service tools
      SinuCom NC, SinuCom ARC, SinuCom FFS,
      SinuCom PCIN and the Commissioning Tool; 
      SW release 7.2

are, effective immediately, released for general availability. It will be supplied on DVD.

With SW release 7.2 of SinuCom NC, the integrated and partially automated acceptance test is now also available for SINUMERIK 840D solution line. The "safe brake test" has been integrated into the SinuCom SI acceptance test as new feature.
The integrated "Commissioning Tool SIMODRIVE 611 digital/SINAMICS S120" was updated to SW release 7.2 SP2.


The SinuCom commissioning and service tools are used for simple commissioning/service of SINUMERIK 810D/840D/840D sl/840Di sl. They have been designed to be used by personnel from the machinery construction OEMs.

Components that have been released:

Description

Order No.

Version

Software SinuCom commissioning and service tools

Software 7.2, single license, on DVD *)
Software 7.2, update, on DVD *)




6FC5250-7AY00-2AG0
6FC5250-7AY00-2AG3




07.02.00.00
07.02.00.00

*) Content of the DVDs:

Component

Version

SinuCom NC(de/en/fr/it/sp)
    
with CT-Editor
            HMI Base

V07.20.10
V01.00.00
V07.20.18

SinuComARC (de/en)

V02.00.03

SinuComFFS (de/en)

V01.01.01

SinuComPCIN (en)

V01.03.03

Commissioning Tool SW 7.2 SP1(de/en/fr/it/sp/v-ch)
incl.
SW 7.2 SP2(install separately)

V07.20.18
V07.20.19

Further software releases:
 - SinuCom Software 6.2 will remain available.
 - SinuCom Software 6.3 will be substituted for 6.4.
 - SinuCom Software 6.4 will remain available.
 - SinuCom Software 7.1 will remain available.
 - Software 7.2 will be supplied for orders entered for the current SW release.

New functions and function improvements with respect to status SinuCom V07.01.02 and Commissioning Tool 7.2 SP1
Also refer to 23335052

SinuComNC:

 -

No changes with respect to SinuCom 07.01.02

 

 

SinuComNC SI acceptance test:

 -

Acceptance test for  SINUMERIK 840D solution line:
The integrated and partially automated acceptance test is now also available for SINUMERIK 840D solution line with SW release 7.2 of SinuCom NC.

 -

Languages for CT-Editor:
The operator interface of the CT-Editor (to generate machine-specific templates) is now available in all 5 standard languages.

 -

Brake test (SBC):
The "safe brake test" has been integrated into the SinuCom SI acceptance test as new point.
Using the trace data display, the following are documented
 - the speed limiting
 - the required torque
 - the actual position
 - the reference drive speed (drive setpoint speed)

 

 

SinuComNC Trace:

 -

No changes with respect to SinuCom 07.01.02

 

 

SinuComARC:

 -

Expansion of the SinuCom ARC functionality for the SINAMICS drive system.

 

 

SinuComFFS:

 -

No changes with respect to SinuCom 07.01.02

 

 

SinuComPCIN:

 -

No changes with respect to SinuCom 07.01.02

 

 

Commissioning ToolSIMODRIVE 611digital/SINAMICS S120:

 -

Expansion of the SINAMICS commissioning
 - filter parameterization
 - automatic speed controller optimization for synchronous motors
 - performance improvements

 -

For all of the improvements, refer to the Upgrade Instructions, Commissioning Tool 7.2 SP2

Prerequisites:
 

 

WIN 95

WIN 98

WIN ME

WIN 2000

WIN NT

WIN XP

SinuCom NC

-

-

-

-

-

Yes

SinuCom FFS

-

-

-

-

Yes

Yes

SinuCom ARC

-

-

Yes

Yes

Yes

Yes

SinuCom PCIN

Yes

Yes

Yes

Yes

Yes

Yes

Commissioning Tool

-

-

-

-

-

Yes

 

"-"

is not supported

 

SinuComNC:

-

Windows XP Prof. SP1 or SP2

-

Can be installed on PC/PG (or alternatively on SINUMERK PCU 50/70 and PCU 50.3 with HMI Adv.)

-

HW minimum requirements: Pentium III with 566 MHz; 512 MB RAM

-

SinuCom NC requires approx. 7MB in the Windows directory and 50 MB in the SinuCom NC directory

-

Recommended display resolution >= 800 x 600

-

NCU system software from 05.01.22; recommended: >= 5.3

-

HMI Advanced or HMI Base from SW release 7.2

SinuComNC SI acceptance test:

-

NCU-SW 810D/840D from SW6.4 Version 06.04.15 and 840D sl from SW1.3 SP2

-

HMI Advanced or HMI Base from SW release 7.2

-

Display resolution >= 800 x 600 and 640 x 480 (for OP 010; with scroll bars)

SinuComNC Trace:

-
-

NCU-SW from 05.03.37 (only for IPO signals)
NCU SW from 06.04.15 (for full functionality)

-

HMI Advanced or HMI Base from SW release 7.2

SinuCom ARC, SinuCom FFS and SinuCom PCIN:

-

Refer to the associated readme file (*.txt)

Commissioning Tool SIMODRIVE 611digital/SINAMIC S120:

-

Commissioning Tool 7.2 can be combined with
 - SINUMERIK 810D/840D from SW6.5
 - SINUMERIK 840D sl from SW1.3 SP2
 - SINUMERIK 840Di sl SW1.1

-

Commissioning Tool 7.2 can only run on Win XP

-

Commissioning Tool 7.2 only supports the "new design"

-

The function "upgrade archive" is no longer available for solution line

Restrictions with respect to Catalog NC61, Edition 2005:

The SinuCom CFS tool to generate CF card images is still not included in this release.

Documentation:
 

-

The documentation for SinuCom NC Edition 08/05 is available in Germany and English on the DVD and can be called-up as online help.

-

The documentation is included as autonomous document 
     SinuCom NC: Commissioning/Service Tool Edition 08/05
on the DOConCD.

Upgrade Instructions, Commissioning Tool SW 7.2 SP2:

siemens_ib_76.rtf ( 37 KB )

Information regarding "Cardware":

Also refer to 21336365

For more detailed information, please contact your local Siemens office.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.