×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 24039110, Entry date: 10/13/2006
(0)
Rate

Which settings have to be defined in order to send text messages (SMS) to an e-mail recipient using SINAUT ST7?

  • Entry
  • Associated product(s)

 
Configuration notes:
If you wish to send a text message to an e-mail address and not, as would ordinarily be the case, to another mobile phone user, the text message starts with the recipient's e-mail address, following by the actual text.
Since the configuration tool does not support the use of the special character "@" in the e-mail address, this has to be replaced by "*".


Fig. 01

 

Enter the destination number of the provider's e-mail gateway in the "SMS DB configuration" of the SINAUT configuration tool instead of the mobile phone number.

The destination numbers for e-mail gateways vary from one provider to the next:
 

Provider E-mail destination number
T-Mobile 8000
D2-Vodafone 3400
Table 01


Fig. 02

 

Note:
In order to use this function, firmware version V4.3.3 at least is required for TIM 3 and TIM 4.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.