Entry type:
FAQ
Entry ID:
24072800,
Entry date:
02/18/2017
Rate
MICROMASTER 4 (MM4), SINAMICS G110 / G120 (CU 2x0x): RS232 / USB Adapter
-
Entry
-
Associated product(s)
My PG/PC has only USB ports. How can I go online to my inverter using USS protocol?
If your PC/PG only has USB interfaces instead of the RS232 interface, you can use standard USB<->RS232 converters. Please make sure that you use up-to-date drivers from the respective manufacturers, particularly also for 64-Bit-Systems.
Note
If data transfer rate problems occur, then the min. baud rate should be set to 38400.
Settings
Drive Monitor | Interface | COM1 - COM4 | A COM port number can be selected between 1-4 (dependent on the PC setting). |
---|---|---|---|
Baud rate | 9600 or higher | A higher baud rate might give the better access; e.g. 38400 Baud | |
Bus operation RS485 | Automatic mode | Online operation is not possible without this setting | |
STARTER | Access point | DEVICE(STARTER, SCOUT) --> PC COM-Port (USS) | |
Interface Parameter Assignment Used | PC COM-Port (USS) | ||
Interface | COM1 - COM7 | A COM port number can be selected between 1-7 (dependent on the PC setting). | |
Baud rate | 9600 or higher | A higher baud rate might give the better access; e.g. 38400 Baud | |
RS485 | Automatic mode | Online operation without this setting is not possible | |
Device Manager | Ports (COM & LPT) | USB<->RS232-Adapter | E.g. ATEN USB to Serial Bridge (COM4) |
Properties of the Port: | |||
Bits per second | 9600 | Leave the presetting's | |
Data bits | 8 | ||
Parity | None | ||
Stop bits | 1 | ||
Flow control | None | ||
COM Port Number | The COM port number can be modified between 1-7 when required |
Information
Further information about interface settings you will find in the attached pdf-file. 24072800_FAQ-DEE6B7DF_USB-RS232_converter_en.pdf (760,2 KB)
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
- Chinese
Entry belongs to product tree folder(s):
- Drive Technology Converters Low voltage converters Standard Performance Frequency Converter SINAMICS G110 Built-In Units
- Drive Technology Converters Low voltage converters Dezentrale Frequenzumrichter SINAMICS G110D Distributed Converters
- Drive Technology Converters Low voltage converters Dezentrale Frequenzumrichter SINAMICS G120D Distributed Converters
- Drive Technology Converters Low voltage converters Standard Performance Frequency Converter SINAMICS G120 Built-In Units Control Units
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 410
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 420
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 430
- Drive Technology Converters Low voltage converters MICROMASTER Frequency Converters MICROMASTER 4 MICROMASTER 440
- Drive Technology Archive converters Low-voltage converters General Performance Umrichter SINAMICS G SINAMICS G110 Built-in units
Rate entry
Feedback *)
Name
Phone number
email
DetailPages.Subject
Comment
Number of characters: 0 (max. 500)
Send copy of comment to sender. (login required)
*) Important: Please use this form for general feedback only. All technical and specialist topics should be directed to the expert community in the Technical Forum.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information