×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 24094737, Entry date: 02/05/2007
(1)
Rate

Technology CPU 317T-2 DP: Cross Slide / Single Belt Application

  • Entry
  • Associated product(s)

Problem 
A two-dimensional positioning is to be performed for an application. A "cross slide" is to be used.
The characteristic feature of this mechanical arrangement is the minimization of the dynamic masses. The two drive units of the "cross slide" do not have to be moved for motion in the plane (XY). The dynamic mass of the "cross slide" is thus reduced to a minimum; this enables to achieve very high accelerations and velocities during the travel motion.

Solution:
The task was realized by using a technology CPU and the "Move 3D" technology template in conjunction with the new "CS_GearIn" function block (CS=CrossSlide).
This entry is realized as an application example, but the "CS_GearIn" function block can, as in technology templates, be used for your own programs.

Function of FB "CS_GearIn":

FB "CS-GearIn" transforms the specified motion in the XY direction into the necessary rotary motions of the axes A1 and A2 of the cross slide. This enables to easily control this kinematics via the selection of the position in the XY plane.

 

Content of Downloads

 

Download
Documentation (German)
 
The accompanying documentation is broken down into three parts: The Introduction part describes the specific automation problem and the suggested solution. The Extension part focuses on imparting in-depth knowledge of the control elements and technological functions. The Demonstration part is aimed at users who intend to demonstrate the functions of the CPU31xT- 2DP or who would like to substantiate their theoretical knowledge through practical testing.
Introduction 24094737_CPU31xT_CrossSlide_Einfuehrung_DOKU_v31_d.pdf ( 355 KB )
Extension 24094737_CPU31xT_CrossSlide_Erweiterung_DOKU_v31_d.pdf ( 989 KB )
Demonstration 24094737_CPU31xT_CrossSlide_Demonstration_DOKU_v31_d.pdf ( 1193 KB )
Documentation (English) 
The accompanying documentation is broken down into three parts: The Introduction part describes the specific automation problem and the suggested solution. The Extension part focuses on imparting in-depth knowledge of the control elements and technological functions. The Demonstration part is aimed at users who intend to demonstrate the functions of the CPU31xT- 2DP or who would like to substantiate their theoretical knowledge through practical testing.
Introduction 24094737_CPU31xT_CrossSlide_Einfuehrung_DOKU_v31_e.pdf ( 338 KB )
Extension 24094737_CPU31xT_CrossSlide_Erweiterung_DOKU_v31_e.pdf ( 1010 KB )
Demonstration 24094737_CPU31xT_CrossSlide_Demonstration_DOKU_v31_e.pdf ( 1211 KB )
Code 
An S7 project as the core element of the demonstration system, consisting of the data for TO parameter setting, the programmed sequences realized with the STEP7 blocks and the WinCC Flexible 2005 user interfaces.

The program archives can be used either without a drive connected or with a SINAMICS S120 Trainings case connected. The required modifications to the program to use the SINAMICS are described in the documentation part Demonstration.

Program Archive 24094737_CPU317T_CrossSlide_v_CODE_v31.zip ( 9761 KB )

 

History

Version

Modification

02/2007 first edition, V3.1 suitable for S7 Technology V3.0 + SP1

 

Keywords:
pick and place, single belt, cross slider, cinematic,

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.