Entry type:
FAQ
Entry ID:
24137746,
Entry date:
01/10/2007
Rate
TPM traffic-light type signals not visible for HMI Adv. V7.x
-
Entry
-
Associated product(s)
QUESTION:
For PCU modules with installed HMI Advanced V7.xx (< V07.03.00.00), when the MCIS TPM is installed, the TPM signal to display the service states is not visible.
ANSWER:
To solve this problem please proceed as follows:
1. Start your PCU in the Windows service mode
2. Copy the zip file attached to this document into a directory / onto a data medium that the Windows system of the PCU can access.
3. Unzip the zip file directly under the directory f:\hmi_adv\icons
For the prompt that possible existing files under f:\hmi_adv\icons will be overwritten, please acknowledge with yes - or yes all.
4. Boot your PCU normally – the traffic-light type symbol should now be displayed.
TPM-icons-ENU.zip ( 15 KB )
For PCU modules with installed HMI Advanced V7.xx (< V07.03.00.00), when the MCIS TPM is installed, the TPM signal to display the service states is not visible.
ANSWER:
To solve this problem please proceed as follows:
1. Start your PCU in the Windows service mode
2. Copy the zip file attached to this document into a directory / onto a data medium that the Windows system of the PCU can access.
3. Unzip the zip file directly under the directory f:\hmi_adv\icons
For the prompt that possible existing files under f:\hmi_adv\icons will be overwritten, please acknowledge with yes - or yes all.
4. Boot your PCU normally – the traffic-light type symbol should now be displayed.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems SINUMERIK CNC Automation System CNC controls SINUMERIK 840 SINUMERIK 840D
- Automation Technology Automation Systems SINUMERIK CNC Automation System Operator components
- Automation Technology Automation Systems SINUMERIK CNC Automation System HMI software for CNC controls Operation and programming
- Automation Technology Automation Systems SINUMERIK CNC Automation System HMI software for CNC controls MCIS Motion Control Information System TPM - Total Productive Maintenance
- Automation Technology Automation Systems SINUMERIK CNC Automation System Related Products and Functions SinuTrain
- Services Training Services Training-related Services SinuTrain SINUMERIK Training Software
Rate entry
Feedback *)
Name
Phone number
email
DetailPages.Subject
Comment
Number of characters: 0 (max. 500)
Send copy of comment to sender. (login required)
*) Important: Please use this form for general feedback only. All technical and specialist topics should be directed to the expert community in the Technical Forum.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information