×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 24229613, Entry date: 12/12/2006
(0)
Rate

How do you configure screen selection on a line or graphics operator panel via controller job 51?

  • Entry
  • Associated product(s)

Instructions:
Proceed as follows to configure screen selection via the controller. At the end of this entry is a free download of a sample program.
 

No. Procedure
1 Create area pointer:
In ProTool you create the area pointer "Interface Area".
The length of 16 words is preset.


Fig. 01
2 Structure of a PLC job:
A PLC job consists of 4 data words. The first data word contains the job number. Depending on the function, up to three parameters are transferred in data words 2 to 4. The figure below shows the principle structure.


Fig. 02

Structure of PLC job 51.


Fig. 03

Detailed information on the topic of area pointers and setting the separate parameters is available in the manual SIMATIC HMI Communication, Appendix B,  "PLC Jobs".
The manual is available in Entry ID 1137086.

3 Functional sequence:
If the first word of the job mailbox is not equal to zero, the operator panel evaluates the PLC job. The operator panel then resets that data word to zero. For this reason the parameters must be entered first in the job mailbox and only then the job number.
4 Sample program:
FC1 coordinates the PLC job. DB51 is the interface block in this case. Using the marker 0.0 "Start_select_screen" you can trigger screen selection once
of "Screen 1" with a positive edge. The marker is reset by FC1.


Fig. 04

The attached download contains the archived STEP 7 project and integrated ProTool project, along with the functions described above.

 Attachment1:  Project_1.zip ( 215 KB )

Runnability and test environment:
The example can be used on all the CPU types of SIMATIC S7-300, S7-400 and WinAC.
The following table lists the components that have been used to create this entry and verify the functions described.
 

Component Product and version designation
PC operating system Microsoft Windows XP SP2
Standard tools STEP 7 V5.3 SP3
Engineering tools -
HMI software ProTool V6.0 SP3
HMI devices OP17 / OP27
Controllers S7 CPU 316-2DP
Table 1: Creation environment of the download attached

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.