×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 24360824, Entry date: 01/05/2007
(0)
Rate

What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?

  • Entry
  • Associated product(s)

Configuration note:
When OPC groups are activated, the OPC DA server loaded with SIMATIC NET PC software CD Edition 2006 is initially only able to return "OPC_QUALITY_WAITING_FOR_INITIAL_DATA=0x20" for items with VT_EMPTY-type data values.

Please ensure that your OPC client supports this return value. Otherwise, your OPC client application needs to be changed accordingly.

Note:
This return value is a valid value according to the OPC specification. 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.