×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 24376232, Entry date: 12/08/2008
(0)
Rate

How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?

  • Entry
  • Associated product(s)

Instructions:
All the information relevant to setting up a teleservice connection between an S7-200 controller and MD 720-3 as Remote Station of a local station based on the Micro Automation Sets 21 (Entry ID: 22537809) is available in the document provided here.

Attachment 1: Teleservice_MD720-3_v1d1_en.pdf ( 1152 KB )

Note:
The SINAUT MD720-3 modem supports both GSM and GPRS communication. For GPRS communication, however, you also need the SINAUT MICRO SC software for the OPC server. For the use of teleservice only, you can also use the GSM modem SIPLUS TC65T (Entry ID: 26955813)

Keywords:
Teleservice, GSM, S7-200 CPU, Controller, MC45, Terminal, Remote connection, Communication, Service, CSD, STEP 7 Micro/WIN 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.