×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 24467314, Entry date: 11/16/2007
(0)
Rate

What are the options for implementing the CP443-1 EX41?

  • Entry
  • Associated product(s)

Configuration notes:
The CP443-1 Advanced with order no. 6GK7443-1EX41-0XE0 can be implemented with the SIMATIC S7-400 CPUs as from firmware version V5.0. According to the delivery release, CP443-1 Advanced with order no. 6GK7443-1EX41-0XE0 can be implemented with restricted range of functions on with SIMATIC S7-400 CPUs as from firmware version V4.x. The delivery release of CP443-1 Advanced with order no. 6GK7443-1EX41-0XE0 is available in Entry ID 24020919.

The attached table provides information on the compatibility of CP443-1 EX41 with SIMATIC S7-400 CPUs as from firmware version V4.x.

SIMATIC_NET_CP443-1_EX41_Kompatibilitaet.pdf ( 7 KB )

Note:
Please note that CP443-1 Advanced (6GK7443-1EX40/41-0XE0) cannot be used with an S7 400 H controller.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.