×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 24843629, Entry date: 01/31/2008
(10)
Rate

Contents of the Installation CD for SIMATIC USB Prommer

  • Entry
  • Associated product(s)

To be able to operate the SIMATIC USB prommer under Microsoft Windows, you require certain drivers. These drivers (also contained on the installation CD ROM supplied with the product) can be downloaded from the links below. If the installation CD ROM gets lost, the drivers are thus easily available for installation. Two different files are available for downloading, depending on the operating system used:

  • CD 10/2007 for the operating systems:
    • MS Windows XP Home
    • MS Windows XP Professional
    • MS Windows Server 2003 (R2 Standard Edition)
    • MS Windows Vista Business (32-bit Edition)
    • MS Windows Vista Ultimate (32-bit Edition)
    • MS Windows Vista Enterprise (32-bit Edition)

 

  • CD 12/2002 for the operating systems:
    • Windows 98SE
    • Windows ME
    • Windows 2000

Please read the relevant installation hints:

Installation hints for CD 10/2007

Installation CD 10/2007 for SIMATIC USB prommer

  1. The contents of the CD has been included in the file

    ( 20954 KB ) USB_Prommer_CD_2007.zip ( 20954 KB ) .
  2. Please unpack the file "USB_Prommer_CD_2007.zip" to a separate directory
  3. Before starting with the installation please close all STEP 7 applications
  4. After unpacking please start the installation by double clicking the file Setup.exe, which is included in "...\USB_Prommer_CD".
  5. If required, the latest Adobe Reader can be downloaded under www.adobe.com .
  6. After the installation has been completed you can connect the USB Prommer to your PC with a USB cable. Please ensure that your memory card interface is set to  "External Prommer" and "USB" connection.

Installation hints for CD 12/2002

Installation CD 12/2002 for SIMATIC USB prommer

  1. The contents of the CD has been included in the file

    ( 76428 KB )  USB_Prommer_CD_2002.zip ( 76428 KB )   
     
  2. Please unpack the file “USB_Prommer_CD_2002.zip“ to a separate directory
  3. Before starting with the installation please close all STEP 7 applications
  4. After unpacking please use the Acrobat Reader to open the file "Welcome.pdf", which is located in "...\USB_Prommer_CD\USB_Prommer_V1.1\".
    Select the required language and start the software installation.
  5. After the installation has been completed you can connect the USB Prommer to your PC with a USB cable. Please ensure that your memory card interface is set to  "External Prommer" and "USB" connection.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.