×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 24847063, Entry date: 03/08/2007
(0)
Rate

SINAUT MICRO SC S7-200 Block Library Update V1.16

  • Entry
  • Associated product(s)
SINAUT MICRO SC S7-200 Block Library Update V1.16

For the purpose of product improvement of the S7-200 block library of SINAUT MICRO SC we are herewith providing a free update.

 

The following function of the PLC Library SINAUT MICRO SC has been improved:
Data higher than the VB adress 5118 can now be dispatched.

Detailed information on the use of the communication software blocks is available from the SINAUT MICRO SC system manual.

Installation of the library:
Please replace the library file sinautmicrosc.mwl by the current version provided for downloading below. How to include a new library is described under entry ID :16689345
 


 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.