Entry type: Download Entry ID: 24947196, Entry date: 07/11/2007
(1)
Rate

IMCEA Driver Download V1.6

  • Entry
  • Associated product(s)

Description

The WINDOWS IMCEA driver permits direct addressing of hardware interfaces under a Microsoft Windows NT / Windows 2000 and Windows XP operating system. For this purpose the following physical I/O resources can be accessed via a C programming interface:

  • Memory-mapped I/Os, e.g. onboard SRAM of the SIMATIC Microbox PC 420
  • Port-based I/Os, e.g. onboard LEDs of the SIMATIC Microbox PC 420
  • Interrupts, e.g. interrupt processing in the case of changes on the monitored inputs of the digital I/O modules of the PC IO central I/O expansion

The WINDOWS IMCEA driver download provides you with two driver versions:

  • WINDOWS IMCEA (PnP): plug-and-play driver for Windows 2000 / XP
  • WINDOWS IMCEA (nPnP): non plug-and-play driver for Windows NT / 2000 / XP

To be able to use the plug-and-play version of the driver your computer requires a PCI/CPCI bus, or a PCI 104/PC104+ interface. The installation file for the plug-and-play driver included in the driver download supports the following I/O modules:

  • SICOMP CPCI-EA221

Version V1.6 and higher:

  • PC IO central I/O expansion for SIMATIC Microbox PC 420 consisting of the following components
    • PC IO BASE 400
    • PC IO MOD DIGITAL 010
    • PC IO MOD ANALOG 020
  • SICOMP CPCI-SFT200 (in the planing stage, based on PC IO BASE 400)
  • SICOMP CPCI-EAM220 (in the planing stage, based on PC IO MOD DIGITAL 010)
  • SICOMP CPCI-EAM230 (in the planing stage, based on PC IO MOD ANALOG 020)

The non plug-and-play driver enables direct access to the onboard resources of SIMATIC PCs and SICOMP IMC modules, e.g. onboard LEDs and onboard SRAM of the SIMATIC Microbox PC 420.

The driver download includes application examples for the use of both driver versions:

  • Non plug-and-play driver:
    Application example for the control of onboard LEDs and onboard SRAM on the SIMATIC Microbox PC 420.
  • Plug-and-play driver:
    Application examples for the control of components of the PC IO central I/O expansion for SIMATIC Microbox PC 420. Access to the analog and digital PC IO MOD modules incl. interrupt operation, as well as the evaluation of an encoder connected to a PC IO BASE module, are shown in three simple programming examples.

System prerequisites

The IMCEA driver can be used with the following Microsoft operating systems:

  • Windows XP
  • Windows 2000
  • Windows NT

Supported PC systems

The following SIMATIC PCs and SICOMP microcomputers are supported by the IMCEA driver:

SIMATIC PCs

  • SIMATIC Box PC 620 V1/V2
  • SIMATIC Box PC 627
  • SIMATIC Box PC 840 V1/V2
  • SIMATIC Rack PC 840 V1/V2
  • SIMATIC Rack PC IL 40 S/V2
  • SIMATIC Rack PC IL 43
  • SIMATIC Microbox PC 420
  • PC IO central I/O expansion for SIMATIC Microbox PC 420

SICOMP IMC

  • SICOMP SMP16-CPU070
  • SICOMP CPCI/SMP16-CPU076
  • SICOMP CPCI/SMP16-CPU086
  • SICOMP CPCI-EA221
  • SICOMP CPCI-SFT200 (in the planing stage, based on PC IO BASE 400)
  • SICOMP CPCI-EAM220 (in the planing stage, based on PC IO MOD DIGITAL 010)
  • SICOMP CPCI-EAM230 (in the planing stage, based on PC IO MOD ANALOG 020)

Installation

Hints on installation are provided in the programming manual.

Download

Contents of the Downloads

Download

Installation instructions / Programming manual (German)

( 3145 KB )  

 

Installation instructions / Programming manual (English)

( 1783 KB )  

 

IMCEA driver V1.6

incl. programming manuals in German and English

( 4885 KB )  

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.