×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 25001302, Entry date: 06/08/2007
(1)
Rate

SIMATIC USB Prommer Firmware Update V1.2.2

  • Entry
  • Associated product(s)

DESCRIPTION:

A change of the USB Prommer firmware has become necessary in order to be able to use the new functions of the STEP 7 software.
Reading out the serial no. of Memory Cards is supported with STEP 7 V5.4 SP2 and higher.

 

Software prerequisites

The SIMATIC USB Prommer firmware V1.2.2 requires the SIMATIC USB Prommer software V1.0 SP1.

Titel of the download

USB_Prommer_FW_V1.2.2.zip ( 224 KB ) ( 224 KB )

Update V1.2.2 for SIMATIC USB Prommer firmware

  1. Please unpack the file "USB_Prommer_FW_V1.2.2.zip" to a separate directory
  2. Before starting with the installation please close all STEP 7 applications
  3. Connect the USB Prommer to your PC via the USB cable. Please ensure that your memory card interface is set to  "External Prommer" and "USB" connection.
  4. After unpacking please start the program "s7ouflsx.exe". Use the dialog "Search for" to select the firmware file "USB_Prommer_FW_V1.2.2.FWL" and start the loading process via the button "Execute". The new firmware will now be programmed in the USB Prommer. You will be given further instructions in the course of the programming process.

Note: If a problem occurres during updating of the SIMATIC USB Prommer firmware, please remove the external voltage supply, remove and return the USB cable to the USB Prommer and execute the firmware update again.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.