×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 25166781, Entry date: 09/01/2011
(7)
Rate

SINAMICS G/S: Toolbox V2.1 / S7 Function Blocks

  • Entry
  • Associated product(s)

DESCRIPTION:

The SINAMICS toolbox comprises a sample project 'Fb283_Bsp_V2_1.zip', which includes an interface block that allows to conveniently connect the SINAMICS converters to PROFIBUS / PROFINET.

This version supports the following converters:

  • SINAMICS G120
  • SINAMICS G120D
  • SINAMICS G130
  • SINAMICS G150
  • SINAMICS S110
  • SINAMICS S120

The function block FB283 allows to transfer all the necessary drive process data. This block is especially suitable for actuating the EPOS functions of the SINAMICS S110 and S120, but it can also be used as a mere speed drive.

Further, the FB283 provides the following functions:

  • The existing drive parameters can be read or overwritten.
  • The fault buffer can be read out.
  • You can transfer up to 64 traversing blocks with one function trigger.
  • Max. 10 arbitrary parameters can be read / written with one job (e.g. to adapt the product).

This S7 function block is documented in the file 'Fb283_V21_ger.PDF', which is also included in the toolbox ZIP file and can be read using the Acrobat Reader.

Toolbox_V21.zip ( 3011 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.