×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 25339612, Entry date: 04/27/2007
(1)
Rate

MICROMASTER: Parameter reading&writing of a MM4 using S7-300/400 (STEP 7 V5) with PROFIBUS Parameter (realtime clock)

  • Entry
  • Associated product(s)

Exclusion:

This application only applies to MICROMASTER 4

 

Task:

This application shows how the time (clock time) of the drive inverter can be synchronized with the CPU clock time - and how you can read-out the fault buffer and the clock time of the drive inverter.

 

Solution:

All drive inverters have an internal time transmitter function that is used to time-stamp and log error conditions. However, there is no battery buffered realtime clock (RTC). The drive inverters can support a software-controlled RTC where the RTC must be set from the AOP or via an interface. When using the AOP, this synchronization is automatically carried-out. When using a serial interface, a request must be sent from the higher-level control to write to parameters.

This example shows how the time transmitter function of the inverter MICROMASTER 4 can be synchronized with the realtime clock of a CPU via PROFIBUS when the drive inverter is powered-up. An S7 project example has been written to achieve this. In the project, the realtime clock of the CPU is read-out and the time is written to parameter P2115 of the drive inverter. The project example also allows the fault buffer of the drive inverter to be read-out and the drive inverter to be controlled.

 


 

Downloads

Content of Downloads

Download

Documentation (German)
Echtzeituhr
PDF_Echtzeituhr_V1_00.pdf ( 1691 KB )
Documentation (English)
Real Time Clock
PDF_Real_time_clock_V1_76.pdf ( 1620 KB )
Code
Real Time Clock
MM4_Real_time_clock_76.zip ( 413 KB )

 

History

Version Date

Modification

V1.0 April 2007 first edition

 

Keywords: Realtime clock, MM4, Step 7, synchronizing

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.