×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 25358470, Entry date: 09/23/2011
(7)
Rate

Function Blocks, Examples and User Manuals of the Serial Interface ET200S 1SI

  • Entry
  • Associated product(s)

 DESCRIPTION:

The function blocks from the libraries support:

Serial Interface Module ET200S ASCII/3964R

Serial Interface Module ET200S  Modbus/USS



Overview of the order numbers and latest versions of the libraries: 

Order Number

Version

6ES7138-4DF01-0AB0

6ES7138-4DF11-0AB0

   
 

V2.5.3:
FB2 - V2.2
FB3 - V2.3
FB81 - V2.2
all others - V2.0

Update Description

 1SI_Disk1_V253.ZIP ( 21565 KB )

 

V2.5.2:
FB2 - V2.2
FB3 - V2.3
FB81 - V2.2
all others - V2.0

Update Description

 1SI_Disk1_V252.ZIP ( 20640 KB )

 

V2.5.1:
FB2 - V2.1
FB3 - V2.3
FB81 - V2.2
all others - V2.0

Update Description

 1SI_Disk1_V251.ZIP ( 20638 KB )

 

V2.3:
FB3 - V2.2
FB81 - V2.2
all others - V2.0

Update Description

 1SI_Disk1_V23.ZIP ( 10553 KB )

  V2.2:
FB3 - V2.2
FB81 - V2.2
all others - V2.0

Update Description

 1SI_Disk1_V22.ZIP ( 11474 KB )

 

V2.1:
FB3 - V2.2
FB81 - V2.1
all others - V2.0

Update Description

 1SI_Disk1_V21.ZIP ( 11474 KB )

6ES7138-4DF00-0AB0

6ES7138-4DF10-0AB0

   
  V1.4

Update Description

 1SI_Disk1_V14.ZIP ( 1152 KB )



Version V2.5.3: Function BlocksFB2 - V2.2 / FB3 - V2.3 / FB81 - V2.2 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • The installation of the "Function Blocks, Examples and User Manuals of the Serial Interface ET200S 1SI" can now also be performed under the operating system Windows 7 / 64-bit.  

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"]. 

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files. 

Version V2.5.2: Function BlocksFB2 - V2.2 / FB3 - V2.3 / FB81 - V2.2 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • Correction of the FB2 to ensure a warm restart of the Modbus communication after return of voltage on the IM (with FB2 - V2.2 or higher only in conjunction with firmware version V1.4.0). 

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"].

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files.

Version V2.5.1: Function BlocksFB2 - V2.1 / FB3 - V2.3 / FB81 - V2.2 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • Readme files and user manuals have been revised (English and German).
  • The modules can now also be operated in a distributed configuration with SIMATIC S7-400 CPUs, if they have been configured with less than 32 bytes of user data (from FB2 - V2.1 / FB3 - V2.3).
  • Write access operations to non-enabled flags or output areas will no longer be executed (from FB81 - V2.2). 

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"]. 

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files.

Version V2.3: Function BlocksFB3 - V2.2 / FB81 - V2.2 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • The installation of the "Function Blocks, Examples and User Manuals of the Serial Interface ET200S 1SI" can now also be performed under the operating system Windows VISTA.

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"]. 

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files.

Version V2.2: Function BlocksFB3 - V2.2 / FB81 - V2.2 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • Prevention of write access operations to non-enabled flags or output areas. 
    The change is only effective in the new version 2.2 of the FB81.

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"]. 

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files.

Version V2.1: Function Blocks FB3 - V2.2 / FB81 - V2.1 / all others - V2.0
(6ES7 138-4DF01-0AB0 / 6ES7138-4DF11-0AB0)



Changes

  • An area length error will be reported, if the parameter LEN is set to zero while the instruction is running.
  • CPUs with a flag area of more than 65,535 bits are supported as well.

Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.2 SP 1 or higher as well as the HW update ET200S 1SI ASCII/3964(R) [corresponds to HSP "s7h0056x.hsp"] or ET200S 1SI Modbus/USS [corresponds to HSP "s7h0058x.hsp"].

NOTES:

  • The instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.
  • The following applies to FBs V2.x or higher: The parameter COM_RST of FBs 2 to 8 (S_RCV, S_SEND, S_VSTAT, S_VSET, S_XON, S_RTS and S_V24) is used to inform the FB of a startup. If you are using one of the above FBs, you must set the respective parameter COM_RST  in the startup OB to 1. Then call the respective FB in cyclic mode without setting or resetting the parameter COM_RST.

Hardware Requirements
The installation of the library, the project examples and the user manuals calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 15 MB of available space on your hard drive for the installation files.

Function Blocks V1.4 (6ES7 138-4DF00-0AB0 / 6ES7138-4DF10-0AB0)


Software Requirements
The use of the function blocks from the libraries requires an installed version of SIMATIC STEP 7 V5.0 or higher. 

NOTE:
These instance data blocks must not be loaded to the CPU during active communication of the SEND/RECEIVE blocks.

Hardware Requirements
The installation of the library calls for the same requirements as the installation of STEP 7. Required in addition:

  • Approx. 1 MB of available space on your hard drive for the installation files. 
  • Support of the following module:
    Serial interface module ET200S
Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.