×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 25392066, Entry date: 05/29/2007
(0)
Rate

ServicePack 3 for D7-SYS V6.2

  • Entry
  • Associated product(s)

DESCRIPTION:

The ServicePack 3 below supports the use of the SIMATIC TDC PROFIBUS CP50M (see entry ID 25093121 and can only be used in conjunction with D7-SYS V6.2.

The following are affected:

  • D7-SYS V6.2 
  • D7-ES V6.2
  • D7-SYS V6.2 Upg.
  • D7-SYS-SFC V6.2
  • D7-ES-SFC V6.2

(6ES7 852-0CC00-0YA5)
(6ES7 852-2CC00-0YA5)
(6ES7 852-0CC00-0YE5)
(6ES7 852-1CC00-0YA5)
(6ES7 852-3CC00-0YA5)

The precondition for the use of ServicePack 3 for D7-SYS V6.2 is CFC V6.1 SP1.

Extensions of ServicePack 3

  • Support of the new SIMATIC TDC PROFIBUS CP50M1 (order no. 6DD1661-0AD1, FW V1.0)

ServicePack 3 for D7-SYS V6.2
 download_sp3_for_v62.zip ( 12844 KB )  

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.