×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 25412338, Entry date: 02/20/2008
(0)
Rate

Manual Input in SIMATIC IT Historian

  • Entry
  • Associated product(s)

The application is a sample solution and shows how manual input (e.g. laboratory values) is entered in SIMATIC IT Historian. It is also illustrated how this process can be monitored with an Audit Trail and an Electronic Signature. The application uses the COM interface of the SIMATIC IT Plant Performance Analyser (PPA), for writing new measured values for measuring locations into the PPA archive.

Downloads

Content of Downloads

Download

Manual Input in SIMATIC IT Historian V6.1 SP1 25412338_Manual_Input_SITHis_V61_en.pdf ( 437 KB )
Manual Input in SIMATIC IT Historian V6.3 SP1 25412338_Manual_Input_SITHis_V63_en.pdf ( 429 KB )
Code for SIMATIC IT Historian V6.1 SP1
Visual Basic Applikation
25412338_Code_V61.zip ( 208 KB )
Code for SIMATIC IT Historian V6.3 SP1
Visual Basic Applikation
25412338_Code_V63.zip ( 198 KB )

 

History

Version

Modification

05/2007 First release
08/2007 update
02/2008 Additional version for SIMATIC IT Historian V6.3 SP1

Keywords
SIT, SITHis

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.