×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 25413978, Entry date: 05/21/2007
(0)
Rate

How can you make the menu item "WinCC" visible again in MS Excel when using the "WinCC Configuration Tool"?

  • Entry
  • Associated product(s)

Instructions:
Despite correct installation of the "WinCC Configuration Tool" or the "WinCC Archive Configuration Tool" these items might be disabled by Excel with the "Automated safe mode" so that the menu items "WinCC" and "WinCC Archive" are not visible.

The Online Help of Microsoft Excel provides information on the "Safe Mode" of Microsoft Office; for example how to re-enable disabled elements.

Proceed as follows to re-enable the WinCC add-ins:
 

No. Description
1 In Excel you select the menu item "Help > About Microsoft Office Excel". The "About Microsoft Excel" window opens.
2 In the "About Microsoft Excel" window click on the "Disabled Items..." button. The "Disabled Items" window opens in which the disabled add-ins are displayed.
3 In the "Disabled Items" list you select the item for the add-in to be activated, e.g. "WinCC", and click on the "Enable" button.
4 You must then restart Excel.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.