×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 25702331, Entry date: 02/28/2011
(3)
Rate

Configuration and Use of the Mobile Panel 277F IWLAN

  • Entry
  • Associated product(s)

Objective of the application:
This application gives the user all configuration steps necessary for generating a project for a ...
  • Mobile Panel 277F IWLAN
  • Mobile Panel 277F IWLAN V2
  • Mobile Panel 277F IWLAN RFID.

This application deals with the following topics:

  • Basic information on the topics
    • Mobile Panel 277F IWLAN
    • IWLAN
    • F-programming
    • rapid roaming
  • Parameterizing an access point (SCALANCE W788-1PRO, SCALANCE W788-2RR)
  • Creating the STEP 7 program and the F-program
  • Creating the Mobile Panel 277F IWLAN program
  • Commissioning the Mobile Panel 277F IWLAN
  • Commissioning the Mobile Panel 277F IWLAN RFID
  • Settings for the "Rapid Roaming" functionality

To get to know the functions of the Mobile Panel 277F IWLAN, the following automation example is used.

In a parcel handover station, a robot picks up parcels from a conveyor and then places them in a compartment (box/rack).
Outside the enclosed protection zone, the conveyor and the robot are operated using the Mobile Panel 277F IWLAN.
For maintenance and settings work, the robot can also be operated in the enclosed protection zone using the Mobile Panel 277F IWLAN.
In case of danger, the conveyor and the robot are switched off via an external emergency stop button or the emergency stop button of the Mobile Panel 277F IWLAN.

Downloads (for the Mobile Panel 277F IWLAN)

No. Content of the Downloads Documentation Standard configuration

Application configuration

1 Configuration and Use
of the Mobile Panel 277F IWLAN
(Incl. parameterization of
SCALANCE W788-1PRO)
25702331_MobilePanel277F_IWLAN_en.pdf ( 4189 KB ) 25702331_Standard_MobilePanel277F_IWLAN.zip ( 3740 KB )
See note for 1)
25702331_Application_MobilePanel277F_IWLAN.zip ( 10525 KB )
See note for 2)

1)    Standard configuration (minimal configuration) of STEP 7 and WinCC flexible configuration
2)   
Standard configuration incl. application extension for STEP 7 and WinCC flexible
 

Downloads (for the Mobile Panel 277F IWLAN V2)

No. Content of the Downloads Documentation Standard configuration

Application configuration

2 Configuration and Use
of the Mobile Panel 277F IWLAN V2
(Incl. parameterization of
SCALANCE W788-1PRO)
25702331_MobilePanel277F_IWLAN_V2_en.pdf ( 5332 KB ) 25702331_Standard_Project_V2_CODE_v20.zip ( 3325 KB )
See note for 1)
25702331_Application_Project_V2.zip ( 10870 KB )
See note for 2)
3 Configuration and Use
of the Mobile Panel 277F IWLAN V2
Expansion by the
"Roaming" functionality
(Incl. parameterization of
SCALANCE W788-2RR)

(Roaming = uninterruptible bridging of larger distances without logon and logoff at different access points)
 
25702331_MobilePanel277F_IWLAN_V2_Roaming_en.pdf ( 2560 KB ) 25702331_Standard_Project_V2_Roaming.zip ( 3320 KB )
See note for 1)
--
4 Configuration and Use
of the Mobile Panel 277F IWLAN V2 Expansion by the application example with RFID tag
(Incl. parameterization of
SCALANCE W788-1PRO)
25702331_MobilePanel277F_IWLAN_RFID_en.pdf ( 3524 KB ) 25702331_Standard_Project_V2_RFID.zip ( 3095 KB )
See note for 3)
--

1)    Standard configuration (minimal configuration) of STEP 7 and WinCC flexible configuration
2)   
Standard configuration incl. application expansion for STEP 7 and WinCC flexible
3)    Standard configuration (minimal configuration) of STEP 7 and WinCC flexible configuration    
       incl. RFID tag
application

Software requirements:
The following software versions were used for implementing the example application.

  • STEP 7 V5.4 SP5
  • WinCC flexible 2008 SP2
  • WinCC flexible 2008 SP2  + HSP (Mobile Panel 277F IWLAN V2)
  • S7 Distributed Safety Programming V5.4 SP5
  • S7 F Configuration Pack V5.5 SP6

History

Version

Modifications

03/2010 First issue
02/2011 Expansion for model series "Mobile Panel 277F IWLAN V2"

Keywords:
zone; effective range; transponder, access point, uninterruptible changeover, Mobile Panel V2,

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.