×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 25863773, Entry date: 08/01/2007
(0)
Rate

BOFE – help in Wizard

  • Entry
  • Associated product(s)
QUESTION:
How can the help be expanded using the Wizard (BOFE)?

ANSWER:
A help was output for the two variables RFP and RTP:

DEF RFP=(R///,"RFP","RFP"///////"Hilfe.pdf",1,"RFP")
DEF RTP=(R///,"RTP","RTP"///////"Hilfe.pdf",2,"RTP")

To do this, pdf and txt files with the same name must be set-up:

Help_uk.txt with the following contents:
;Name pdf file; index; page in the pdf file
HILFE.PDF; 1; 1
HILFE.PDF; 2; 1

The help texts "RFP" and "RTP" with a description are provided in the associated pdf file (Hilfe_uk.pdf). Both files must be located in
\cus\hlp.dir
\cma\hlp.dir or
\cst\hlp.dir.

Additional entries are not required.
(refer to the attached example)

pack-ENU.zip ( 46 KB )
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.