×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 26233208, Entry date: 04/25/2018
(236)
Rate

SINAMICS MICROMASTER STARTER

  • Entry
  • Associated product(s)
This contains the last two STARTER versions and additive SINAMICS Support Packages:

Description

This contains the last two STARTER versions and additive SINAMICS Support Packages:

OSS note on SINAMICS MICROMASTER STARTER V5.3 HF1

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
 Registrierung notwendig  OSS_Information_V53.zip (577,8 KB)

SHA-512 ckecksum:  Registrierung notwendig  OSS_V5.3_sha512zip.txt (1 KB) 

Information about SHA-512: 109483101 

Special note for resellers

The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V53.zip


SINAMICS MICROMASTER STARTER V5.3 HF1 SW download

This contains version V5.3 HF1 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS MICROMASTER STARTER V5.3 HF1 (current version)


SINAMICS MICROMASTER STARTER
V5.3 HF1

(Delivery release: 2019-01-17)

 Registrierung notwendig  Vol_1_STARTER_V53_HF1_Program_G110_G120.zip (1,9 GB)

SHA-512 checksum:
  Registrierung notwendig  Vol_1_5301_sha512zip.txt (1 KB)

 See also description for installation versions.

Optional:

 Registrierung notwendig  Vol_2_STARTER_V53_HF1_SSPs_Rest_of_SINAMICS_Family.zip (629,2 MB)

SHA-512 checksum:   Registrierung notwendig  Vol_2_5301_sha512zip.txt (1 KB)

Optional: 

 Registrierung notwendig  Vol_3_STARTER_V53_HF1_HELPS.zip (1,3 GB) 

SHA-512 checksum:  Registrierung notwendig  Vol_3_5301_sha512zip.txt (1 KB)

Associated sales information under 109762379 

SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key.

However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Article number: 6SL3072-0AA00-0AG0.

STARTER V5.3 HF1 supports the languages:

  • German
  • English
  • French
  • Spanish
  • Italian

Details on the supported drive systems (incl. FW versions) can be found in the following overview.

  Installed_Devices_STARTER_DVD_53000100.pdf (401,7 KB) 

Installation versions

In order to save download time and data volume, this STARTER version V5.3 HF1 can also be downloaded and installed WITHOUT online help and WITHOUT SINAMICS S/SINAMICS integrated drives. If you do not want to use the online help, then select the "Minimized" download version.

Installation/download version

Complete, i.e. including online help and all SINAMICS drives
Download file

SINAMICS partial range, i.e. including online help and only with MICROMASTER 4 and SINAMICS G110 and G120
Download file

SINAMICS partial range and minimized, i.e. WITHOUT online help and only with MICROMASTER 4 and SINAMICS G110 and G120
Download file

Vol_1_STARTER_V53_HF1_Program_G110_G120.zipYESYESYES
Vol_2_STARTER_V53_HF1_SSPs_Rest_of_SINAMICS_Family.zipYESNONO
Vol_3_STARTER_V53_HF1_HELPS.zipYESYESNO

Installation procedure for STARTER V5.3 HF1

  1. Download the Vol_1_.. and optional Vol_2_.. and optional Vol_3_.. attached ZIP file(s) (depending on the selected download version).
  2. Unpack the ZIP files into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folder.
  3. After unpacking, the common file folder must appear as follows (shown for the "complete" version):
    \...\CommonFileFolder\01_Readme\
    \...\CommonFileFolder\HELP\
    \...\CommonFileFolder\InstData\
    \...\CommonFileFolder\SSP_BT\
    \...\CommonFileFolder\SSP_DCM\

    \...\CommonFileFolder\SSP_FAMILY\
    \...\CommonFileFolder\SSP_G110_G120\
    \...\CommonFileFolder\SSP_HELP\
    \...\CommonFileFolder\SSP_MV\
    \...\CommonFileFolder\SSP_SIMOTION_INTEGRATED\
    \...\CommonFileFolder\SSP_SINUMERIK_INTEGRATED\
    \...\CommonFileFolder\Unsupported Tools\
  4. Start the STARTER setup program by calling it from ..\SETUP.EXE.

The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.

The restrictions of STARTER V5.3 HF1 you can find here: 109750851.



OSS note on SINAMICS MICROMASTER STARTER V5.1 SP1 HF2 (previous version)

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
 Registrierung notwendig  OSS_Information_V51_SP1.zip (2,0 MB)

SHA-512 ckecksum:  Registrierung notwendig  OSS_V5.1.1_sha512zip.txt (1 KB)

Information about SHA-512: 109483101

Special note for resellers

The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V51_SP1.zip


SINAMICS MICROMASTER STARTER V5.1 SP1 HF2 SW download  (previous version)

This contains version V5.1 SP1 HF2 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS MICROMASTER STARTER V5.1 SP1 HF2 (previous version)


SINAMICS MICROMASTER STARTER
V5.1 SP1 HF2

(Delivery release: 2018-04-24)

 Registrierung notwendig  Vol_1_STARTER_V51_SP1_HF2_Program_G110_G120.zip (1,7 GB)

SHA-512 checksum:
 Registrierung notwendig  Vol_1_HF2_sha512zip.txt (1 KB) 

 See also description for installation versions.

Optional:

 Registrierung notwendig  Vol_2_STARTER_V51_SP1_HF2_SSPs_Rest_of_SINAMICS_Family.zip (554,8 MB)

SHA-512 checksum:
 Registrierung notwendig  Vol_2_HF2_sha512zip.txt (1 KB)

Optional: 

 Registrierung notwendig  Vol_3_STARTER_V51_SP1_HF2_HELPS.zip (1,1 GB) 

SHA-512 checksum:

 Registrierung notwendig  Vol_3_HF2_sha512zip.txt (1 KB)

Associated sales information under 109757244 

SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key.

However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Article number: 6SL3072-0AA00-0AG0.

STARTER V5.1SP1 HF2 supports the languages:

  • German
  • English
  • French
  • Spanish
  • Italian

Details on the supported drive systems (incl. FW versions) can be found in the following overview.

  Installed_Devices_STARTER_DVD_51010200.pdf (343,0 KB) 

Installation versions

In order to save download time and data volume, this STARTER version V5.1 SP1 HF2 can also be downloaded and installed WITHOUT online help and WITHOUT SINAMICS S/SINAMICS integrated drives. If you do not want to use the online help, then select the "Minimized" download version.

Installation/download version

Complete, i.e. including online help and all SINAMICS drives
Download file

SINAMICS partial range, i.e. including online help and only with MICROMASTER 4 and SINAMICS G110 and G120
Download file

SINAMICS partial range and minimized, i.e. WITHOUT online help and only with MICROMASTER 4 and SINAMICS G110 and G120
Download file

Vol_1_STARTER_V51_SP1_HF2_Program_G110_G120.zipYESYESYES
Vol_2_STARTER_V51_SP1_HF2_SSPs_Rest_of_SINAMICS_Family.zipYESNONO
Vol_3_STARTER_V51_SP1_HF2_HELPS.zipYESYESNO

Installation procedure for STARTER V5.1 SP1 HF2

  1. Download the Vol_1_.. and optional Vol_2_.. and optional Vol_3_.. attached ZIP file(s) (depending on the selected download version).
  2. Unpack the ZIP files into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folder.
  3. After unpacking, the common file folder must appear as follows (shown for the "complete" version):
    \...\CommonFileFolder\01_Readme\
    \...\CommonFileFolder\HELP\
    \...\CommonFileFolder\InstData\
    \...\CommonFileFolder\SSP_BT\
    \...\CommonFileFolder\SSP_DCM\

    \...\CommonFileFolder\SSP_FAMILY\
    \...\CommonFileFolder\SSP_G110_G120\
    \...\CommonFileFolder\SSP_HELP\
    \...\CommonFileFolder\SSP_MV\
    \...\CommonFileFolder\SSP_SIMOTION_INTEGRATED\
    \...\CommonFileFolder\SSP_SINUMERIK_INTEGRATED\
    \...\CommonFileFolder\Unsupported Tools\
  4. Start the STARTER setup program by calling it from ..\SETUP.EXE.

The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.

The restrictions of STARTER V5.1 SP1 HF2 you can find here: 109750851.

Important information on SINAMICS G120 with FW Version >= V4.7 SP3:

  • With the SINAMICS Firmware Version V4.7 SP3 (see 109476414), the commissioning wizard for Control Units G120 with PM240, PM240-2 and PM330, as well as for G120C has been reworked. The three new SINAMICS application classes Standard and Dynamic Drive Control as well as Expert are offered, which are automatically preset in accordance with the SINAMICS G120 power unit used. The SINAMICS application classes simplify commissioning and ensure rugged motor control. For this, a motor data identification is performed once when switching on the drive for the first time.
Warning

If a motor data identification routine (motor ID) with subsequent run-up to the setpoint speed is selected (p1900 = 11 or 12; 12 = standard setting for "Standard Drive Control" and "Dynamic Drive Control"), then, with the first switch-on command, after a short delay time, caused by the motor ID (approx. 8 to 30 sec), the motor is immediately accelerated up to the setpoint speed. For further information, see 109480663.

To be able to use the revised commissioning wizard, it is absolutely necessary to upgrade the STARTER to Version >= V4.4 SP1.      

  • Note on SIMOTION SCOUT V4.5
    SCOUT V4.5 behaves correspondingly like STARTER >= V4.4 SP1.


Overview and links to the SINAMICS Support Packages (SSPs)

SSP, SINAMICS G120 (G110M, ET 200pro FC-2) see 109477753

SSP, SINAMICS S120 (S150, G130, G150) see 109477641

SSP, SINAMICS S110 V4.4 SP3 see 109476277

SSP, SINAMICS DCP V1.1 see 109474935

SSP, SINAMICS DCM V1.4 SP1 see 44029688

SSP, SINUMERIK SINAMICS Int V4.7: Installation only within framework of STARTER V4.4 SP1!

SSP, SINAMICS G120P BT see 109478085.


Note regarding the download

As a result of the security settings, as shown in the screenshot, the download can be classified as a security risk. In order to avoid problems after the installation, ZIP files after the download must be classified as harmless by right clicking on > Properties > "Allow" button.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.