SINAMICS STARTER
-
Entry
-
Associated product(s)
Description
Here you will find the last two current STARTER versions and their associated updates (HF), as well as the links to the SINAMICS Support Packages:
OSS note on SINAMICS STARTER V5.4 SP2 HF1 (current version)
Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
OSS_Information_V5421.zip (21,9 MB)
SHA-512 ckecksum:
OSS_V5421_sha512zip.txt (1 KB)
Information about SHA-512: 109483101
Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V5421.zip
SINAMICS STARTER V5.4 SP2 HF1 SW download (current version)
Hint according STARTER integrated at STEP 7 >= V5.7 (for applications with SIMATIC S7) and STARTER Standalone:The function "Monitoring the application integrity" is supported from STARTER V5.4 SP2 HF1. Please also see the product note entry for STEP 7 V5.7: 109794088
An update (V5.4 SP2 HF2)) is available for this STARTER version! The download please see table of contents.
This contains version V5.4 SP2 HF1 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.
SINAMICS STARTER V5.4 SP2 HF1 (current version) | |
---|---|
SINAMICS STARTER (Delivery release: 2021-07-30) |
SHA-512 checksum:
|
Associated sales information under 109800526
SINAMICS STARTER can be used free of charge without entering a license key.
However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DL-DVD. Article number: 6SL3072-0AA00-0AG0.
STARTER V5.4 SP2 HF1 supports the languages:
- German
- English
- French
- Spanish
- Italian
Details on the supported drive systems (incl. FW versions) can be found in the following overview.
Installed_Devices_STARTER_DVD_54020100.pdf (459,6 KB)
Installation procedure for STARTER V5.4 SP2 HF1
- Download both ZIP files.
- Unpack the both ZIP files into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folders.
- After unpacking, the common file folder must appear as follows:
\...\CommonFileFolder\01_Readme\
\...\CommonFileFolder\03_Manuals_SINAMICS_DCC\
\...\CommonFileFolder\04_dcblib\
\...\CommonFileFolder\HELP\
\...\CommonFileFolder\InstData\
\...\CommonFileFolder\Unsupported Tools\ - Start the STARTER setup program by calling it from ..\SETUP.EXE.
The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.
The restrictions of STARTER V5.4 SP2 HF1 you can find here: 109750851.
Hotfix 2 for SINAMICS STARTER V5.4 SP2 HF1
For STARTER version V5.4 SP2 HF1, this hotfix 2 is provided as a so-called Add On Setup.
- Commissioning
of third-party motors not possible as of Starter V5.4 HF2 with SINAMICS
firmware V5.2 SP3
Malfunction: When commissioning third-party motors, the "automatic calculation" P340 = 3 is automatically set when certain parameters are entered. When this is the case, other necessary parameters can no longer be entered and the configuration cannot be completed. (Error number: 213865)
- Possible computer crash of STARTER V5.4 SP2 HF1 during the function:
Activate online mode (via VPN connection)
Due to a certain SW component version, a computer crash (Windows blue screen) may occur when the online mode is activated. (Error number: 290912)
- Problem configuring multiple drive data sets with STARTER V5.4 SP SP2
HF1
Drive no longer changes to Ready after the number of DDS is extended (Error number: 286520)
Important note:
After installing this Hotfix 2, you must reinstall the current SSP SINAMICS S120 (S150, G130, G150) V5.2 SP3 109477641 to ensure error-free selection of motors.
For this STARTER Hotfix 2, the OSS information of version V5.4 SP1 HF1 is still valid (see above).
Here you will find the SINAMICS STARTER V5.4 SP2 HF2:
SINAMICS STARTER V5.4 SP2 HF2 | |
---|---|
SINAMICS STARTER (Delivery release: 2021-12-20) |
SHA-512 checksum: |
Installation procedure:
- Download the ZIP file.
- Unpack the ZIP file into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folder.
- Start the STARTER setup program by calling it from ..VOL1\SETUP.EXE.
The installation runs automatically through the following phases:
- The setup checks your computer for an existing STARTER installation.
- If version V5.4 SP2 HF1 of the STARTER is found, Hotfix 2 will also be installed.
- If no STARTER version or another version is found, the setup is aborted.
The readme file contains important information.
OSS note on SINAMICS MICROMASTER STARTER V5.4 HF2 (previous version)
Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
OSS_Information_V5402.zip (20,5 MB)
SHA-512 ckecksum:
OSS_V5402_sha512zip.txt (1 KB)
Information about SHA-512: 109483101
Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.
Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V5401.zip
SINAMICS MICROMASTER STARTER V5.4 HF2 SW download (previous version)
Important hint according STARTER integrated in STEP 7 >= V5.7 (for applications with SIMATIC S7):
Please note the programm message according the monitoring of application integrity. See also the product note entry for STEP 7 V5.7: 109794088
This contains version V5.4 HF2 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.
SINAMICS MICROMASTER STARTER V5.4 HF2 (previous version) | |
---|---|
SINAMICS MICROMASTER STARTER (Delivery release: 2020-11-04) |
SHA-512 checksum: See also description for installation versions. |
Associated sales information under 109782792
SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key.
However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Article number: 6SL3072-0AA00-0AG0.
STARTER V5.4 HF2 supports the languages:
- German
- English
- French
- Spanish
- Italian
Details on the supported drive systems (incl. FW versions) can be found in the following overview.
Installed_Devices_STARTER_DVD_54000200.pdf (471,9 KB)
Installation procedure for STARTER V5.4 HF2
- Download the ZIP file.
- Unpack the ZIP file into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folder.
- After unpacking, the common file folder must appear as follows:
\...\CommonFileFolder\01_Readme\
\...\CommonFileFolder\HELP\
\...\CommonFileFolder\InstData\
\...\CommonFileFolder\Unsupported Tools\ - Start the STARTER setup program by calling it from ..\SETUP.EXE.
The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.
The restrictions of STARTER V5.4 HF2 you can find here: 109750851.
Overview and links to the SINAMICS Support Packages (SSPs)
SSP, SINAMICS G120 (G110M, ET 200pro FC-2) see 109477753
SSP, SINAMICS S120 (S150, G130, G150) see 109477641
SSP, SINAMICS S110 V4.4 SP3 see 109476277
SSP, SINAMICS DCM V1.4 SP1 see 44029688
SSP, SINUMERIK SINAMICS Int V4.7: Installation only within framework of STARTER V4.4 SP1!
SSP, SINAMICS G120P BT see 109478085.
Note regarding the download
As a result of the security settings, as shown in the screenshot, the download can be classified as a security risk. In order to avoid problems after the installation, ZIP files after the download must be classified as harmless by right clicking on > Properties > "Allow" button.

- German
Entry belongs to product tree folder(s):
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry