×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 26233208, Entry date: 08/02/2021
(292)
Rate

SINAMICS STARTER

  • Entry
  • Associated product(s)
This contains the last two STARTER versions and additive SINAMICS Support Packages:

Description

This contains the last two STARTER versions and additive SINAMICS Support Packages:


OSS note on SINAMICS STARTER V5.4 SP2 HF1 (current version)

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
 Registrierung notwendig  OSS_Information_V5421.zip (21,9 MB)

SHA-512 ckecksum:  Registrierung notwendig  OSS_V5421_sha512zip.txt (1 KB)

Information about SHA-512: 109483101 

Special note for resellers

The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V5421.zip


SINAMICS STARTER V5.4 SP2 HF1 SW download (current version)

Hint according STARTER integrated at STEP 7 >= V5.7 (for applications with SIMATIC S7) and STARTER Standalone:
The function "Monitoring the application integrity" is supported from STARTER V5.4 SP2 HF1. Please also see the product note entry for STEP 7 V5.7: 109794088 

This contains version V5.4 SP2 HF1 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS STARTER V5.4 SP2 HF1 (current version)


SINAMICS STARTER
V5.4 SP2 HF1

(Delivery release: 2021-07-30)

 Registrierung notwendig  STARTER_V54_SP2_HF1_Programm_Part_1.zip (3,8 GB)

SHA-512 checksum:  Registrierung notwendig  Part_1_V5421_sha512zip.txt (1 KB)

 Registrierung notwendig  STARTER_V54_SP2_HF1_Programm_Part_2.zip (1,2 GB)

SHA-512 checksum: Registrierung notwendig  Part_2_V5421_sha512zip.txt (1 KB)
 

Associated sales information under 109800526  

SINAMICS STARTER can be used free of charge without entering a license key.

However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DL-DVD. Article number: 6SL3072-0AA00-0AG0.

STARTER V5.4 SP2 HF1 supports the languages:

  • German
  • English
  • French
  • Spanish
  • Italian

Details on the supported drive systems (incl. FW versions) can be found in the following overview.

 Registrierung notwendig  Installed_Devices_STARTER_DVD_54020100.pdf (459,6 KB)


Installation procedure for STARTER V5.4 SP2 HF1

  1. Download both  ZIP files.
  2. Unpack the both ZIP files into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folders.
  3. After unpacking, the common file folder must appear as follows:
    \...\CommonFileFolder\01_Readme\
    \...\CommonFileFolder\03_Manuals_SINAMICS_DCC\
    \...\CommonFileFolder\04_dcblib\
    \...\CommonFileFolder\HELP\
    \...\CommonFileFolder\InstData\
    \...\CommonFileFolder\Unsupported Tools\
  4. Start the STARTER setup program by calling it from ..\SETUP.EXE.

The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.

The restrictions of STARTER V5.4 SP2 HF1 you can find here: 109750851.


OSS note on SINAMICS MICROMASTER STARTER V5.4 HF2 (previous version)

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
 Registrierung notwendig  OSS_Information_V5402.zip (20,5 MB)

SHA-512 ckecksum:  Registrierung notwendig  OSS_V5402_sha512zip.txt (1 KB) 

Information about SHA-512: 109483101 

Special note for resellers

The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file Open_Source_Software.zip in the OSS_Information_V5401.zip


SINAMICS MICROMASTER STARTER V5.4 HF2 SW download (previous version)

Important hint according STARTER integrated in STEP 7 >= V5.7 (for applications with SIMATIC S7):
Please note the programm message according the monitoring of application integrity. See also the product note entry for STEP 7 V5.7: 109794088 

This contains version V5.4 HF2 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS MICROMASTER STARTER V5.4 HF2 (previous version)


SINAMICS MICROMASTER STARTER
V5.4 HF2

(Delivery release: 2020-11-04)

 Registrierung notwendig  STARTER_V54_HF2_Programm.zip (3,6 GB)

SHA-512 checksum:
  Registrierung notwendig  V54_HF2_sha512zip.txt (1 KB)

 See also description for installation versions.

Associated sales information under  109782792 

SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key.

However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Article number: 6SL3072-0AA00-0AG0.

STARTER V5.4 HF2 supports the languages:

  • German
  • English
  • French
  • Spanish
  • Italian

Details on the supported drive systems (incl. FW versions) can be found in the following overview.

 Registrierung notwendig  Installed_Devices_STARTER_DVD_54000200.pdf (471,9 KB)


Installation procedure for STARTER V5.4 HF2

  1. Download the  ZIP file.
  2. Unpack the ZIP file into a common target file folder on your hard disk. Please ensure that there are no spaces in the entire path name of this target file folder.
  3. After unpacking, the common file folder must appear as follows:
    \...\CommonFileFolder\01_Readme\
    \...\CommonFileFolder\HELP\
    \...\CommonFileFolder\InstData\
    \...\CommonFileFolder\Unsupported Tools\
  4. Start the STARTER setup program by calling it from ..\SETUP.EXE.

The readme file contains important information on how to use the tool. The links for the SINAMICS FW restrictions you can find in the readme file.

The restrictions of STARTER V5.4 HF2 you can find here: 109750851.




Overview and links to the SINAMICS Support Packages (SSPs)

SSP, SINAMICS G120 (G110M, ET 200pro FC-2) see 109477753

SSP, SINAMICS S120 (S150, G130, G150) see 109477641

SSP, SINAMICS S110 V4.4 SP3 see 109476277

SSP, SINAMICS DCP V1.1 see 109474935

SSP, SINAMICS DCM V1.4 SP1 see 44029688

SSP, SINUMERIK SINAMICS Int V4.7: Installation only within framework of STARTER V4.4 SP1!

SSP, SINAMICS G120P BT see 109478085.


Note regarding the download

As a result of the security settings, as shown in the screenshot, the download can be classified as a security risk. In order to avoid problems after the installation, ZIP files after the download must be classified as harmless by right clicking on > Properties > "Allow" button.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.