Entry type: Download, Entry ID: 26233208, Entry date: 06/15/2015
(35)
Rate

SINAMICS MICROMASTER STARTER

  • Entry
  • Associated product(s)
This contains the last two STARTER versions and additive SINAMICS Support Packages:

DESCRIPTION

This contains the last two STARTER versions and additive SINAMICS Support Packages:

 

SINAMICS MICROMASTER STARTER V4.4 SP1

This contains version V4.4 SP1 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS MICROMASTER STARTER V4.4 SP1 (actual version)

SINAMICS MICROMASTER STARTER V4.4 SP1 (Release for general availability: 10.06.2015)

Associated sales information 109476613

  Vol_1_STARTER_V44_SP1_Program_G110_G120.zip (1,2 GB) 

optionally:

  Vol_2_STARTER_V44_SP1_SSPs_Rest_of_SINAMICS_Family.zip (719,1 MB)

optionally:

  Vol_3_STARTER_V44_SP1_HELPS.zip (1,0 GB)

 

SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key. However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Order number: 6SL3072-0AA00-0AG0.

STARTER V4.4 SP1 supports

  • German
  • English
  • French
  • Spanish
  • Italian.

Details on the supported drive systems can be found in the following Excel overview.

  Installed_Devices_STARTER_DVD_44010000.pdf (19,9 KB)

 

Installation versions
In order to save download time and data volume, this STARTER version V4.4 SP1 can also be downloaded and installed WITHOUT online help and WITHOUT SINAMICS S/SINAMICS integrated drives. If you do not want to use the online help, then select the "Minimized" download version.

Installation/download version

Complete,
i.e. download
all SINAMICS drives
files including online help

SINAMICS partial range,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
including online help

SINAMICS partial range and minimized,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
WITHOUT online help

Vol_1_STARTER_V44_SP1_Program_G110_G120.zip

YES

YES

YES

Vol_2_STARTER_V44_SP1_SSPs_Rest_of_SINAMICS_Family.zip

YES

NO

NO

Vol_3_STARTER_V44_SP1_HELPS.zip

YES

YES

NO

Procedure to install STARTER V4.4 SP1:

  1. Download the 1 or 2 or 3 attached ZIP files (depending on the selected download version)
  2. Unpack the ZIP files into a shared target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory.
  3. After unpacking, the shared directory must appear as follows (shown for the "complete" version):
    \...\GemeinsamesVerzeichnis\01_Readme\
    \...\GemeinsamesVerzeichnis\CD_1\
    \...\GemeinsamesVerzeichnis\CD_2\
    \...\GemeinsamesVerzeichnis\CD_3\
    \...\GemeinsamesVerzeichnis\SSP_BT\
    \...\GemeinsamesVerzeichnis\SSP_DCM\
    \...\GemeinsamesVerzeichnis\SSP_FAMILY\
    \...\GemeinsamesVerzeichnis\SSP_G110_G120\
    \...\GemeinsamesVerzeichnis\SSP_HELP\
    \...\GemeinsamesVerzeichnis\SSP_MV\
    \...\GemeinsamesVerzeichnis\SSP_SIMOTION_INTEGRATED\
    \...\GemeinsamesVerzeichnis\SSP_SINUMERIK_INTEGRATED\
    \...\GemeinsamesVerzeichnis\Unsupported Tools\
  4. Start the STARTER setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool.  

 

 

 

SINAMICS MICROMASTER STARTER V4.4 HF3

Important hint for STARTER usage together with SINUMERIK:
Please do not use the Hotfix 3 version of STARTER V4.4 together with SINUMERIK devices.
For this scenario please use STARTER version V4.4 or use versions >= V4.4 SP1.
Please see information at the article 103929354.

 

This contains version V4.4 HF3 of the STARTER commissioning tool for the SINAMICS, SIMATIC ET200 FC and MICROMASTER 4 drive systems.

SINAMICS MICROMASTER STARTER V4.4 HF3 (previous version)

SINAMICS MICROMASTER STARTER V4.4 HF3 (Release for general availability: 24.10.2014)

Associated sales information Item ID 103929354.

  vol_1_starter_v44_hf3_program.zip (852,6 MB)

  vol_2a_starter_v44_hf3_ssps_g110_g120.zip (222,9 MB)

 

optionally:

  vol_2b_starter_v44_hf3_ssps_rest_of_sinamics_family.zip (578,2 MB)

optionally:

  vol_3_starter_v44_hf3_helps.zip (1,4 GB)

 
SINAMICS MICROMASTER STARTER can be used free of charge without entering a license key. However, for legal licensing reasons, you should be in possession of a STARTER license certificate (any version). If this is not the case, you can also order the current STARTER version including license certificate on a DVD. Order number: 6SL3072-0AA00-0AG0.

STARTER V4.4 HF3 supports

  • German
  • English
  • French
  • Spanish
  • Italian.

Details on the supported drive systems can be found in the following Excel overview.

Installation versions
In order to save download time and data volume, this STARTER version V4.4 HF3 can also be downloaded and installed WITHOUT online help and WITHOUT SINAMICS S/SINAMICS integrated drives. If you do not want to use the online help, then select the "Minimized" download version.

Installation/download version

Complete,
i.e. download
all SINAMICS drives
files including online help

SINAMICS partial range,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
including online help

SINAMICS partial range and minimized,
i.e. only download MICROMASTER 4 and SINAMICS G110 and G120
WITHOUT online help

Vol_1_STARTER_V44_HF3_Program.zip
Vol_2a_STARTER_V44_HF3_SSPs_G110_G120.zip

YES

YES

YES

Vol_2b_STARTER_V44_HF3_SSPs_Rest_of_SINAMICS_Family.zip

YES

NO

NO

Vol_3_STARTER_V44_HF3_HELPS.zip

YES

YES

NO

Procedure to install STARTER V4.4:

  1. Download the 2 or 3 or 4 attached ZIP files (depending on the selected download version)
  2. Unpack the ZIP files into a shared target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory.
  3. After unpacking, the shared directory must appear as follows (shown for the "complete" version):
    \...\GemeinsamesVerzeichnis\01_Readme\
    \...\GemeinsamesVerzeichnis\CD_1\
    \...\GemeinsamesVerzeichnis\CD_2\
    \...\GemeinsamesVerzeichnis\CD_3\
    \...\GemeinsamesVerzeichnis\SSP_BT\
    \...\GemeinsamesVerzeichnis\SSP_DCM\
    \...\GemeinsamesVerzeichnis\SSP_FAMILY\
    \...\GemeinsamesVerzeichnis\SSP_G110_G120\
    \...\GemeinsamesVerzeichnis\SSP_HELP\
    \...\GemeinsamesVerzeichnis\SSP_MV\
    \...\GemeinsamesVerzeichnis\SSP_SIMOTION_INTEGRATED\
    \...\GemeinsamesVerzeichnis\SSP_SINUMERIK_INTEGRATED\
    \...\GemeinsamesVerzeichnis\Unsupported Tools\
  4. Start the STARTER setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool. 

 

Overview and links to SINAMICS Support Packages (SSP)

 

SSPs for updating existing STARTER resp. SCOUT installations
 
SSP, SINAMICS G120 (G110M, ET200pro FC-2) see 109477753
SSP, SINAMICS S120 (S150, G130, G150) see 109477641
SSP, SINAMICS S110 V4.4 SP3 see 109476277
SSP, SINAMICS DCP V1.1 see 109474935
SSP, SINAMICS DCM V1.4 SP1 see 44029688
SSP, SINUMERIK SINAMICS Int V4.7: Installation only with STARTER V4.4 SP1!
SSP, SINAMICS G120P BT see 109478085

 

Download note

Due to security settings, a download - as marked in the screenshot - may be classified as a security risk.
To avoid problems after the installation, zip files must be classified as harmless after downloading by clicking with right mouse button > Properties > "Unblock" button